Recent discussions
Can't find the soldering peak reflow and also MSL documents for the 1EDN7550U gate driver on the product web page. There is a good board assembly app note with soldering guidelines, but customer is looking for the peak reflow specification.
Please send, thank you!
Gordy Carlson
Infineon PSS FAE
Show LessI am designing a peltier controller, I will use a MOSFET h-bridge for this.
I have been reviewing many data sheets and I have a doubt, I don't know which of these gate drivers to use.
These are the options I would like to use:
a.- 2ED2103S06F
b.- WCDSC006.
I will place 4 N-MOSFET, IRF40R207, on the h-bridge.
I will use a microcontroller from the XMC1400 family that works with 5V for the PWM and the PWM will have a frequency of 5KHz, and calculate that I need a gate resistance of approximately 80 Ohms. I want to use a 12V power supply with the 2ED2103S06F, but I'm not sure if it will turn on the MOSFET fast enough running at 5KHz (it's a relatively low frequency but it's the first time I've worked with infineon's drivers) or maybe it would be better use a WCDSC006 and use a 5V supply, but according to the graph of the IRF40R207 it can handle approximately 12A with a VG of 5V, but the pelier cell that I will use consumes 8.2A and I do not think it is good that the mosfet controls a very close maximum current to the load current.
thanks for your help
I'm working with 1ED3860MC12MXUMA1 gate driver.
I read the manual about the I2C command but without understand well.
Is it possible to have or to receive a link where I can find information and examples about the I2C command. ??
The Gate driver doesn't work and I don't know why.... I need examples of code. I2c.
Thanks in advance
Silvano
Show LessHello,
The utilisation of the ir2010pbf is unclear for me . They is 2 GND , one for Vss (numerical partp and one for the COM (mosfet part). Does these 2 GND must be connected together or are they really isolared (like for example octocouplers).
Greatd regards , Deso
Show Less
Hello there,
I am attempting to run a Altium SPICE simulation with the SPICE model for the IRS21876S, and I'm encountering a few errors. I keep getting a PWL error about an ngspice expression not being a constant. This confused me since there is no PWL source in the model. I'm not sure if this is a problem with the model or Altium, but I thought I'd post this here to help track down the issue. I've included a screenshot of the error messages with this post.
Altium/ngspice Error Messages
Hi
I like the IR4426/7/8 low end drivers because they have MOSFET end stages, have two channels, and have a SO8 package. Unfortunate, the data specifications only specify the pulsed output currents. I need to know what the DC current capacity is.
Can anyone tell me what the DC output current capabilities are of these drivers, and what the RDSon resistance is of the output stage.
Thanks
Show Less
ご担当者様
いつもお世話になっております。
Gate Driver(1ED3491MC12M)の出力電圧スペックに関して、アドバイス頂ければと思います。
データシートP34記載の「High level output voltage」ですが、Vvcc2+0.87 Vとあります。
出力電圧が電源電圧よりも上がるのはなぜでしょうか?
お手数かけ致しますが、ご教示頂ければと思います。
■データシートURL
以上、宜しくお願い致します。
Show LessDear IFXer,
We new have following the 1ED020I12 recommended circuit to design desat function for SIC MOSFET.
but find abnormal waveform need your help, because the issues cause the trigger the fault. And may I know the Vdesat spike root cause is what? how to avoid it? please advise us.
CH1 : Vgs_M
CH2 : Vdesat_M
CH3 : Vds_M
CH4 : OUT
Show Less
Hi community, hi Infineon support,
we are planning to use the AUIR324x IC gate driver for a battery switching architecture with current constraints of
15A continous, 20A for 2mns, 30A for 10s. We have been testing the "AUIR3241S/AUIR3242S - Board Back to Back 12V" with the batteries and it seems to switch correctly between the 2 batteries.
However at this time we have 2 questions :
- technical : attached TEK0000 (GPIO, Load - resistive electronic 150W load - voltage switching from BAT1=13V to BAT2=20V in ~30us) we can see a first intermediate voltage level for 10us then a small peak at 25V before reaching 20V. Could you explain the signal ?
- commercial : we don't see any stock for AUIR324x IC chip and we want to design a PCB around September. What is the expected planning for procurement of this chip ?
Xavier.
Show Less