Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Gate Driver ICs Forum Discussions

Recent discussions

Sort by:
studiosipa
Gate Driver ICs
I'm working with 1ED3860MC12MXUMA1 gate driver.  I read the manual about the I2C command but without understand well.  Is it possible to have or to re... Show More
CaelebMcKee
Gate Driver ICs
Hello there, I am attempting to run a Altium SPICE simulation with the SPICE model for the IRS21876S, and I'm encountering a few errors. I keep gettin... Show More
Piet_de_Pad
Gate Driver ICs
Hi I like the IR4426/7/8 low end drivers because they have MOSFET end stages, have two channels, and have a SO8 package. Unfortunate, the data specifi... Show More
YuTa_4942221
Gate Driver ICs
ご担当者様 いつもお世話になっております。 Gate Driver(1ED3491MC12M)の出力電圧スペックに関して、アドバイス頂ければと思います。 データシートP34記載の「High level output voltage」ですが、Vvcc2+0.87 Vとあります。 出力電圧が電源電圧より... Show More
KUOWENYUNG
Gate Driver ICs
Dear IFXer, We new have following the 1ED020I12 recommended circuit to design desat function for SIC MOSFET.  but find abnormal waveform need your hel... Show More
akshay1305
Gate Driver ICs
eagle model
Solved
Hello,    Can anyone pass the link for eagle model of gate driver auirs2191s.    Regards,  Akshay Show More
xavier1111
Gate Driver ICs
Hi community, hi Infineon support, we are planning to use the AUIR324x IC gate driver for a battery switching architecture with current constraints of... Show More
User21797
Gate Driver ICs
Hi there, As topic, I have went through the whole manual but there is nearly no description about these ov uv err: The most related info I can find i... Show More
nkoekemoerneels
Gate Driver ICs
2ED2410-EM
Solved
HI All Please advise if there is a workbook available to calculate all the requirements for the 2ED2410 driver  Spreadsheet based would be preferable ... Show More
taewan
Gate Driver ICs
Hello infineon I am Kim, a student studying in Korea.One challenge was encountered while implementing a motor drive system.IPTC015N10NM5 is used as a ... Show More
Forum Information

Gate Driver ICs

Every switch needs a driver – the right driver makes a difference. Find your perfect driver with help from our community on our more than 500 EiceDRIVER™ gate driver IC solutions suitable for any power switch, and any application.