Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Gate Driver ICs Forum Discussions

Translation_Bot
Gate Driver ICs
User Guide below p.20" 3.1.4 Overcurrent Protection" V_ITRIP=0.5V, R19=1kΩ, R20=11.3kΩ, Even if it is calculated with Rshunt = 10 mΩ, Iocp is 23.17A i... Show More
Sriram_07
Gate Driver ICs
Hello, We are looking for an isolated gate driver with 5A peak current rating and we came across your 1ED3461MC12M gate driver. We have a few question... Show More
VGS_MLN
Gate Driver ICs
Ladies and Gentlemen, We are using the IR2103SPBF to realise a totem pole stage for ohmic/inductive loads with two N-channel MOSFETs. This is working ... Show More
Translation_Bot
Gate Driver ICs
When I used the 1ED010i12-F2 to drive the SiC MOSFET (C3M0075120D), I had a problem with gate current oscillation. The red waveform is shown below, an... Show More
Translation_Bot
Gate Driver ICs
The SCDL voltage setting range of the TLE7189f chip is 0.7-2.5v. How is the short circuit protection current actually designed by the chip calculated ... Show More
nike3
Gate Driver ICs
Hello Community, I need to implement the SPI functionalities for the 1EDI2002AS on an Infineon AURIX TC397 TFT. Sadly I could not find any library for... Show More
Alex80
Gate Driver ICs
Hi. I'm looking for IR2104 or IR2184 chips DIP8. Help me choose an original product based on photo and price. https://www.aliexpress.com/item/1005006418154585.html... Show More
JiKo_85813
Gate Driver ICs
EVAL-1ED3890Mx12MとEVAL-1ED38x0DCTを使用し、ダブルパルス試験を行おうとしているのですが、 USBがGUI上でもPCのデバイスマネージャー上でも認識されなくなったため、困っています。 EVAL-1ED38x0DCTで短絡が発生している可能性が高そうですが、解決策がござい... Show More
MeysamSaeedian
Gate Driver ICs
Hi,  I have an H-bridge in my design, driving a resistive load using Infineon technologies gate driver (PN: 1ED3491MU12MXUMA1), and SIC MOSFETs with P... Show More
Noraneko_0901
Gate Driver ICs
Regarding the AUIR2181S gate driver, some online trading companies list it as a discontinued product. However, when I checked this product on Infineon... Show More
Forum Information

Gate Driver ICs

Every switch needs a driver – the right driver makes a difference. Find your perfect driver with help from our community on our more than 500 EiceDRIVER™ gate driver IC solutions suitable for any power switch, and any application.