Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Gate Driver ICs Forum Discussions

User19408
Gate Driver ICs
I'm going to use IRS2011 to dirve IRF250P225. I see the in the typical diagram in IRS2011 datasheet,how can I determine the capacitor and diode type ... Show More
User20701
Gate Driver ICs
If i refer the data sheet of IR2181 and attached an image of the ratings and characteristics. I see huge current values of 100A etc. These are very hi... Show More
User20620
Gate Driver ICs
IR11672ASPBF, after the EN pin is turned off, the output is floating, high impedance, low?Hello, everyone,I am currently designing IR11672ASPBF for AC... Show More
Anonymous
Gate Driver ICs
Hello,I am trying to setup a half bridge simulation with IR 2113 and IPx60R125 devices. I have a boot strap circuit and have also charged the capacito... Show More
The_BOOM
Gate Driver ICs
We only need a unipolar positive DC voltage. Can the IRA2153SD work with a simple two-winding transformer and a full-bridge rectifier?What are the dra... Show More
The_BOOM
Gate Driver ICs
Which dual gate drivers can deliver 5V at 2A continuous on each output? Any of these?https://www.infineon.com/cms/en/product/power/gate-driver-ics/galvanic-isolated-gate-driver/?filterValues=~(350_nom~(~2)~290_114_nom~(leftBound~2~rightBound~13.5))&visibleColumnIds=name,opn,productStatusInfo,orderOnline,496_nom,290_114_nom,290_113_nom,350_nom,358,551,852,347,851,608,packageName,640_nom,157_nom,853_min,853_max,853_nom,854_min,854_max,855_nom,856_nom,859_149_nom,860_150_nom#!products Show More
The_BOOM
Gate Driver ICs
For the circuit below, do you recommend a transformer or coupled inductor? Show More
The_BOOM
Gate Driver ICs
about the IR2153D.On the datasheet there's a chart called "IR2153 RT vs Frequency". It shows frequency as high as 1 MHz. But the table called "Electri... Show More
User17665
Gate Driver ICs
Gate drivers
solved msg Solved
What gate drivers can be used for CoolSiC mosfet devices?
User16691
Gate Driver ICs
Hello to all!I would like to know if the driver 1ED020I12-B2 can handle 3 IGBT Infineon FF200R12KT4 ( 3 IGBT for each channel ).It will be used in a f... Show More
Forum Information

Gate Driver ICs

Every switch needs a driver – the right driver makes a difference. Find your perfect driver with help from our community on our more than 500 EiceDRIVER™ gate driver IC solutions suitable for any power switch, and any application.