Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Gate Driver ICs Forum Discussions

Translation_Bot
Gate Driver ICs
refer the title or subject (in an online forum)smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E9%97%A8%E7%BA%A7%E9%A9%B1%E5%8A%A8%E5%99%A8/%E8%AF%B7%E5%B... Show More
kanji_shibatani
Gate Driver ICs
  Dear Team, I am sorry to have a fundamental question. Should I warn (change) about CDESAT value in case Half Bridge or Full-Bridge ? I think DESAT d... Show More
Youcef_RZ
Gate Driver ICs
I hope this message finds you well. I am reaching out to seek clarification regarding a specification mentioned in the datasheet of the IR2109(4)(S) c... Show More
Ankit1
Gate Driver ICs

I am facing an issue while using this IC. IC is not giving proper output to turn on the MOSFET.

alonsoatx
Gate Driver ICs
engineer
solved msg Solved
Will the 1EDN7136G gate driver do 100% duty cycle? Per the simulation it can. But per the datasheet it is unclear. I'm looking for a way to keep the G... Show More
bookhsw
Gate Driver ICs
你好!         请问为啥高侧快关的延时在1us到2us,图中示波器红外是高侧HIN,蓝色是H out的波形,存在延时。黄色是对应低侧(L out),导致存在mos管导通,电流大的情况。请问怎么解决?   Show More
johnzielinski
Gate Driver ICs

Is there a function replacement for the IR2085S.  Customer working on a Commercial AC application.

CVCW
Gate Driver ICs
What power output is the 2EDN7524F FET driver capable of?I need to generate a 1MHz 20V p-p square wave into 50 Ohms. This is a current of just 400mA d... Show More
petbernt
Gate Driver ICs
Hello, I am trying to configure two 1edi2002as devices in a daisy chain configuration for three phases, so six devices in total. I am able to configur... Show More
Engin_TANRIKULU
Gate Driver ICs
Hello, I am using a circuit for motor control. GateDrive is on fire, I think this is a hardware problem. Can you examine the circuit?   Show More
Forum Information

Gate Driver ICs

Every switch needs a driver – the right driver makes a difference. Find your perfect driver with help from our community on our more than 500 EiceDRIVER™ gate driver IC solutions suitable for any power switch, and any application.