Gate Driver ICs Forum Discussions
I have two shipments of some Photovoltaic Relay PVT422Spbf. The product marked as "836P" matches the datasheet drawing and looks original. The product marked as "1120" does't match the datasheet because some of the dimensions do not match.
The datasheet I used is from June 02, 2015 if I am not mistaken. Can you please tell me if there is a newer revision of that document for the PVT422Spbf?
I understand that it is impossible to give a confirmation of the originality of the products from the photo. But could you please tell me if the PVT422S product marked as "1120" could be similar to the original?
All materials in the attachment. Thank you in advance.
Best regards,
Eugene
Show LessHi,
We are using the Gate Driver IC part 1ED3122MU12HXUMA1 to Turn OFF the 1.2kV rated N-Channel MOSFET.
During the High voltage Testing (1usec Pulse width, 1.2kV voltage switching at MOSFET), Gate driver output getting false Turn OFF.
Gate Driver output wave form does not comply with Gate Driver Input wave form.
I have attached two images (Normal Working Condition and False condition). In wave form denotes Yellow Color - Gate Driver Output , Blue Color - Gate Driver Input.
What could be the reason for this False Output ?
Kindly clarify this False Triggering scenario to rectify this issue.
Regards,
Gurusamy M (+91 9842897485)
Data Patterns (I) Ltd,
Chennai-603103, INDIA
Show LessHello everyone,
I am making improvements to a complete h-bridge circuit, I want the PWM signal frequency to be 200kHz and to be able to control duty cycles as small as 1%, ie t_on_PWM = 0.05us, but I think I could use two ICs of the EiceDRIVE 2EDi family, ICs 2EDF9275FXUMA1 and 2EDF7275KXUMA2 seem to be good choices, the problems I'm having are:
1.- Will I be able to use any of the gate controllers mentioned above or are there other better options for my requirements?
2.- What MOSFET could I use for this application? The MOSFETs must be able to switch at the PWM frequency and have a drain current Id > 11A and Vds > 33V and I would also like them to be small since I want to integrate the entire circuit on a 10cm x 10cm PCB.
I hope you can help me. Thank you
Show Less
6ED2742S01Q has an internal LDO for charge pumps and VCC, what is the maximum output current rating for this internal regulator? It's not stated in datasheet.
Thank you.
Show Less
In the BPA Motor control GUI software (v1.3.0 64bit), using the stand-alone configurator, the PWM MODE configuration register, related to the configuration "1PWM with hall sensor", displays the message "not possible due to interconnections - do not use" (see image attached). Can you explain to me the problem?
Show Less1. Trying to load the provided configuration file with the EvalBoardSoftware and get a "Unhandled exception has occurred" error.
2. Unable to select any Gate driver ... the drop-down box is grayed out ... might be related to 1. Is there a valid config file?
John Hooker
Show LessIn the 1EDI60I12AF driver datasheet, it said the input to output isolation voltage (GND2) is +/-1200V. what's that means?
is it the isolation voltage according to UL1577? or something else?
Show LessHello IFXer,
I have question about 1ED31xxMC12H.
With bipolar supply 15V / -8V design,
1. the transformer need use center tap for bipolar supply voltage?
2. could you help us to provide the reference design for iso-power?
3. the VEE2 has absolute maximum ratings? if reference center tap.
Show Less
Infineon introduces the MOTIX three-phase gate driver IC 6ED2742S01Q. What's so special about this chip?
Hello. Thanks for your previous valuable advice, my PCB is working great. There is a small problem about Vitrip+, according to the datasheet I refer to, Vitrip = Idc.R0(R1/R1+ R2) R0 = 0.05R; R1=5.1k; R2=6k (you see the picture on the left below) with Idc=22A we get Vitrip = 0.5V. But the current R0 (shunt resistor) has a very small power, which cannot withstand 22A current. If I use 0.002R shunt resistor it can handle 22A current, but with R0=0.002R I can't figure out reasonable R1 and R2 to feed Vitrip+=0.5V. Refer to "EVAL-6ED2231S12TM1 User Manual" I see that you guys use 3.3v external voltage, so I want a new design to use. So I want to ask you if my design (bottom right picture) is correct?. Thanks a lot
Show Less