Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Gate Driver ICs Forum Discussions

Adam_Shap
Gate Driver ICs
I am writing to seek assistance regarding an issue I am facing with the IRS25752LPBF High-Side Gate Driver, which I recently purchased from Infineon u... Show More
kanji_shibatani
Gate Driver ICs
  Hello Both of AUIR21814S/IR2184S are ' Not for new design'... I could not find  similar product in Home Page.  :600V  :SOIC14N  :source/sink: 1.9A/2... Show More
JPBledsoe
Gate Driver ICs
Hello, I'm new to the gate driver community. Have a question for the community. I've been using Vishay SUP70101EL P-Channel MOSFETs (https://www.vishay.com/docs/77632/sup70101el.pdf... Show More
Yong
Gate Driver ICs
Hi Expert, If I wnat to use TLE92108 in ASIL-B system, what kind of functional safety material can you provide? And do we need external circuit or ext... Show More
LingchangJin
Gate Driver ICs
I would like to use TLE9183 charge pumper for external driver power, to driving an external reverse battery NMOSFET protection, which required max 3mA... Show More
LingchangJin
Gate Driver ICs
1.) From TLE9183 datasheet, there is applicaiton circuit but not mark the parameter of external resistor and capacitor. Would you please give the reco... Show More
vamsi
Gate Driver ICs
Hi, Actually we are using 1ED3124MU12H gate driver IC but in that Active miller clamp protection is not available.  Can you please suggest the gate dr... Show More
Adam_Shap
Gate Driver ICs
Hello, everyone in the community. This is a description of my troubles trouble shooting and finding ways to use IRS25752LPBF IC.  I hope this message ... Show More
Roarzsq
Gate Driver ICs
Hello, I use a microcontroller with an I/O port output of 3.3V to drive IGBT normally through 1EDC60H12AH, and the VCC1 is 5V. However, the logic inpu... Show More
adityasids2010
Gate Driver ICs
This pertains to the solution on Command I2c 1ED3860MC12MXUMA1  A part of the code from the link above is pasted below. Query: How can 0x07 be written... Show More
Forum Information

Gate Driver ICs

Every switch needs a driver – the right driver makes a difference. Find your perfect driver with help from our community on our more than 500 EiceDRIVER™ gate driver IC solutions suitable for any power switch, and any application.