Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Gate Driver ICs Forum Discussions

Sort by:
Jayj30ng
Gate Driver ICs
Hello  I'm trying to Switch battery Power which has 19.2 ~ 21.6V / pK 400A / nominal Max 200A  And trying to use 12 X IRF7480 with AUIR3241S driver   ... Show More
HuTer
Gate Driver ICs
Hello,I'm not able to download the Pspice model for IR2110 from the website, " the web site encountered an error." Anyone can help? Thanks,   Show More
yuhua
Gate Driver ICs

您好,想选择一款支持6Mhz~8MHz频率,可驱动2路或4路mosfet的栅极驱动IC,驱动的mosfet可集成在IC内部也可分离的,有推荐吗?谢谢!

Jerome_S
Gate Driver ICs
AUIR2085S
Solved
Hello, I received a component with following information written on it: A2085 / A441P / IR / C / STX3. I suppose it was manufactured in the 41st week ... Show More
tonywill
Gate Driver ICs
Hello, 1. Digikey discribes this ic as 'IC IGBT DVR 1200V DSO8' however there is  no mention of it being able to drive an IGBT in the datasheet. It on... Show More
User16464
Gate Driver ICs
Just a note for other users, I recently changed from using an IRS2110 (lower floating voltage version) and encountered a persistent fault in an H-bri... Show More
JINHOON
Gate Driver ICs
HI, all. I want to ask whether AUIR3240S can be applied to back-to back FET configuration as AUIR3241S. I don't see back-to-back configuration in AUIR... Show More
User17583
Gate Driver ICs
Hi,I am using IR21814S for LLC gate driver, and I need to limit the minimum duty of PWM signal. Could you help address the minimum HI/LI on pulse req... Show More
User18242
Gate Driver ICs
I have attached the circuit. I'm trying to drive a coolgan HEMT (IGOT60R070D1) with driver - 1EDF5673F.PROBLEM - 1) When I tested the driver alone (w... Show More
Lixiaojuan
Gate Driver ICs
hello, We have used TLE9183 in our design,now I am writing DFEMA,I am confused on what will happen to this IC when two pins of this driver IC short to... Show More
Forum Information

Gate Driver ICs

Every switch needs a driver – the right driver makes a difference. Find your perfect driver with help from our community on our more than 500 EiceDRIVER™ gate driver IC solutions suitable for any power switch, and any application.