Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Gate Driver ICs Forum Discussions

Translation_Bot
Gate Driver ICs
This is about the gate driver of 2ED2181S06F. This is an existing product with a built-in bootstrap diode, but does it also have a limiting resistor b... Show More
mukeshp11
Gate Driver ICs
Hello All,   We are using 1ED020I12-F2 gate driver for driving three phase inverter with 6 IGBT modules and each IGBT module is being driven by 1ED020... Show More
J_Kurano
Gate Driver ICs
I would like to do a simulation that includes the current sense amplifier.Unfortunately, it is not included in the TLE9210x-232QX PSpice Simulation Mo... Show More
nehaagarwal1996
Gate Driver ICs
Hi, I am trying to connect the infineon gate driver for high voltage GaN MOSFET and I have designed the attached Altium circuit. Can you tell me what ... Show More
ivankovi
Gate Driver ICs
  Vinp is pulse source with 3V amplitude. there is no output at OUTB. do you see any error on simulation schematic that stops 2EDF8275 to give OUT B ... Show More
Translation_Bot
Gate Driver ICs
  Hello   Do you have  alternate device or solution for ir2520dpbf? (obsolete) This product seems special , so that  I could not find  alternate... Pl... Show More
salmanpy
Gate Driver ICs
I want to know whether the resistor used in the HIN and LIN is a pull-down resistor or resistor used for limiting the current to the input pins. (Refe... Show More
choulia1
Gate Driver ICs
TLE9183QK电机驱动芯片,工作在正常模式(INH,SOFF,ENA 3个引脚输入3.3V高电平) 当IL1引脚输入10KHZ 50%占空比 PWM波(IH1引脚保持缺省的高电平,关闭上管),GL1为什么不输出对应的PWM波开关对应的下管,保持为低电平?检查ERR引脚输出为正常的3.3V高电平,... Show More
mngr05
Gate Driver ICs
Hello everyone, I am working with the 6ED2231S12TM1 with the IMC101 in order to drive a FP75R12N2T7BPSA1.The 6ED2231S12TM1 is rated for current +0.35A... Show More
adityasids2010
Gate Driver ICs
I had previously raised a query related to the programming of 1ED3860MC12MXUMA1. I received help from the Infineon community in the form of a sample c... Show More
Forum Information

Gate Driver ICs

Every switch needs a driver – the right driver makes a difference. Find your perfect driver with help from our community on our more than 500 EiceDRIVER™ gate driver IC solutions suitable for any power switch, and any application.