- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
hi , fine today
What's the difference between 1EDc(certified insulation ) and 1EDi (galvanic insulation) ?
please send me good idea
Solved! Go to Solution.
- Labels:
-
Gate Driver IC's
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
You can find it in this way. In attached Selection Guide page 12 is a table containing the information you need to find. You can determine the isolation rating of the corresponding product based on the typical values of the input and output currents, the voltage class and the type of isolation. For example, 1EDI05I12AH is functional isolation, the voltage class is 1200V, the typ. Io+/Io- is 1.3A/0.9A. Then the voltage rating is VISO = ± 1200 V.
BR,
Steven
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
thanks for your teaching
that mean, electrical spec is same 1EDc and 1EDi
but 1EDc is certified by the UL
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
You could say they use the same technology (coreless transformer). However, there may be differences in specific electrical properties, such as isolation type, isolation rating or peak drive current.
Steven
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
thanks , thanks
I have a datasheet of AN2014-06 1EDC/1EDI Compact family technical description.
this datasheet don't have a isolation rating, peak drive current.
where can I find this.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi, this AN e includes an explanation of general gate driver input and output features, and
a description of how to use them in an application. It also contains peak drive current, which is called Min. peak output current in the documentation. Please refer to the datasheet of each driver for the specific isolation parameters, which will be described in detail. For example:
BR,
Steven
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
You can find it in this way. In attached Selection Guide page 12 is a table containing the information you need to find. You can determine the isolation rating of the corresponding product based on the typical values of the input and output currents, the voltage class and the type of isolation. For example, 1EDI05I12AH is functional isolation, the voltage class is 1200V, the typ. Io+/Io- is 1.3A/0.9A. Then the voltage rating is VISO = ± 1200 V.
BR,
Steven