- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
I like the IR4426/7/8 low end drivers because they have MOSFET end stages, have two channels, and have a SO8 package. Unfortunate, the data specifications only specify the pulsed output currents. I need to know what the DC current capacity is.
Can anyone tell me what the DC output current capabilities are of these drivers, and what the RDSon resistance is of the output stage.
Thanks
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @Piet_de_Pad ,
Below data is with regards to your initial query.
Rdson_source =6.5 Ω (typ.)
RDS_on_sink= 4.6 Ω (typ.).
The DC current is limited by the power dissipation of the package.
Coming back to your application, kindly allow us sometime to analyse and get back with better solution, if there is any.
Regards
Meghana
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @Piet_de_Pad ,
Thank you for using the Infineon developer community.
Can you please let me know, how are you intending to use this data?
Regards
Meghana R
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Infineon, Meghana
The IR4426/7/8 is DUAL LOW SIDE DRIVER SOIC8 with a MOSFET Totem Pole output. There are not many TTL in to rail to rail output products that have an 1Amp output that can switch voltage above 5V, this chip can do 20V. I wanted to use your chip not as high power MOSFET gate driver but as a TTL level in and power output High Low driver for various loads with continues sink and source currents. Right now I create my own drivers using transistors like the voltage inverter image attached and below, but i don't like this transistor solution.
I hope the IR4426/7/8 can handle equal or more than 1Amp 20V. If you have suggestions for better solution in a SOIC-8 package, I would like to hear that. Your data sheet doesn’t indicate the constant current DC capabilities of the IR4426/7/8 Output and that is why I was asking.
Hope this clears up the reason why I ask my question.
Regards Oscar Goos
Alias Piet_de_Pad
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @Piet_de_Pad ,
Below data is with regards to your initial query.
Rdson_source =6.5 Ω (typ.)
RDS_on_sink= 4.6 Ω (typ.).
The DC current is limited by the power dissipation of the package.
Coming back to your application, kindly allow us sometime to analyse and get back with better solution, if there is any.
Regards
Meghana
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks Meghana,
6.5 and 4.7 Ω That quite high for my application. But it's an answer I can work with.
I f you know a SOC8 with two channels and a mosfet outputs power drivers with a VCC > 5V let me now I havent found them.
Thanks for you help
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @Piet_de_Pad ,
All gate drivers within Infineon portfolio come with MOSFET based output drive stage.
If you need a simple drive control with two channels, IR25600S can be one alternate.
But there are also a few other 2-channel drivers which come with one floating output channel which makes it compatible for driving both a high side and a low side power switch, but since you need them as TTL stage, you can still consider them as well. Please refer below link.
Regards
Meghana R