Level 1
User20927
Level 1
Jan 06, 2021
03:27 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I use IR2110S.
I use only the high side to drive the motor.
Sometimes the motor will not run.
The schematic and oscilloscope waveform are attached.
VBS is measured with a differential probe.
The output of HO gradually drops and reaches 0V. (Cannot be seen on the scale of the attached image)
VBS suddenly becomes 0V.
I have some ideas:
• The duty ratio of the input to HIN is about 98%.
• The motor may have an effect.
I'm in trouble because the problem isn't solved.
I use only the high side to drive the motor.
Sometimes the motor will not run.
The schematic and oscilloscope waveform are attached.
VBS is measured with a differential probe.
The output of HO gradually drops and reaches 0V. (Cannot be seen on the scale of the attached image)
VBS suddenly becomes 0V.
I have some ideas:
• The duty ratio of the input to HIN is about 98%.
• The motor may have an effect.
I'm in trouble because the problem isn't solved.
Solved! Go to Solution.
1 Solution
Moderator

Moderator
Jan 08, 2021
08:57 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
As VBS is going down to 0 V the HO output is switching off. The recharging of the bootstrap capacitor is load dependent and 98% duty cycle is not helping.
You can test with an isolated 12 V power supply across C162 and verify that this is root cause and then try with lower duty cycle (25%)
If you plan to use only the high side, you can look at high-side only gate drivers such as IR2117/8, IR2125 or IR2127.
You can test with an isolated 12 V power supply across C162 and verify that this is root cause and then try with lower duty cycle (25%)
If you plan to use only the high side, you can look at high-side only gate drivers such as IR2117/8, IR2125 or IR2127.
1 Reply
Moderator

Moderator
Jan 08, 2021
08:57 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
As VBS is going down to 0 V the HO output is switching off. The recharging of the bootstrap capacitor is load dependent and 98% duty cycle is not helping.
You can test with an isolated 12 V power supply across C162 and verify that this is root cause and then try with lower duty cycle (25%)
If you plan to use only the high side, you can look at high-side only gate drivers such as IR2117/8, IR2125 or IR2127.
You can test with an isolated 12 V power supply across C162 and verify that this is root cause and then try with lower duty cycle (25%)
If you plan to use only the high side, you can look at high-side only gate drivers such as IR2117/8, IR2125 or IR2127.