Announcements

Register now for the most anticipated Asia Pacific Power Seminar 2022

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Gate Driver ICs Forum Discussions

User20532
Level 1
First solution authored
Level 1
Hello,

When I use the model pspice for the IR2110 for a full bridge I got overflow error. Does someone have a solution to this problem ?

I tried a lot of tweak with the solver, try to use initial condition on various capacitor... But no found solution !

Thanks a lot !

Regards.







0 Likes
1 Solution
AZIZ_HASSAN
Moderator
Moderator 100 sign-ins 50 solutions authored 10 likes received
Moderator

Hi,

I am recommending you few steps and try whether it works or not.

1) Remove load and check the output  voltage.

2) Since, two half bride are connected parallel across DC bus, try to remove one and check the pulse output.

3) If these don't work then there might be a issue with your time signals ( either delay or any other timing signal) .

 

BR,

AZIZ HASSAN

View solution in original post

0 Likes
5 Replies
Srivatsa
Moderator
Moderator 5 sign-ins 50 replies posted 25 solutions authored
Moderator
Hi,

You can provide an initial value to the bootstrap capacitors C17, C23 and check if the error is resolved.

Thanks.
0 Likes
User20532
Level 1
First solution authored
Level 1
Hi,

Thanks you for helping me. I tried but got same error :

0 Likes
Srivatsa
Moderator
Moderator 5 sign-ins 50 replies posted 25 solutions authored
Moderator
What is the deadtime between HIN and LIN? Try with a delay between the two and with 50% duty cycle, LIN first and then HIN.
Try removing the RC across the MOSFETs and the RC at the load L.
0 Likes
MarshallKenn
Level 1
5 sign-ins First reply posted First question asked
Level 1

IR2110/ir2113 Hi, hope this help 🤗

0 Likes
AZIZ_HASSAN
Moderator
Moderator 100 sign-ins 50 solutions authored 10 likes received
Moderator

Hi,

I am recommending you few steps and try whether it works or not.

1) Remove load and check the output  voltage.

2) Since, two half bride are connected parallel across DC bus, try to remove one and check the pulse output.

3) If these don't work then there might be a issue with your time signals ( either delay or any other timing signal) .

 

BR,

AZIZ HASSAN

0 Likes