Announcements

Register now for the most anticipated Asia Pacific Power Seminar 2022

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Gate Driver ICs Forum Discussions

The_BOOM
Level 2
First like received 5 likes given 5 sign-ins
Level 2
Which dual gate drivers can deliver 5V at 2A continuous on each output? Any of these?

https://www.infineon.com/cms/en/product/power/gate-driver-ics/galvanic-isolated-gate-driver/?filterV...
0 Likes
1 Solution
Srivatsa
Moderator
Moderator 5 sign-ins 50 replies posted 25 solutions authored
Moderator
All these can provide 2 A continuous drive current. The 2ED - F2 will not be able to deliver 5 V since the undervoltage lockout of the secondary side is set at 12 V. Hence minimum the recommended output voltage is around 15 V.

2EDF7275F is a 4 V -versions for logic-level MOSFETs and only this driver can deliver 5 V at 2 A continuous on each output.

View solution in original post

0 Likes
1 Reply
Srivatsa
Moderator
Moderator 5 sign-ins 50 replies posted 25 solutions authored
Moderator
All these can provide 2 A continuous drive current. The 2ED - F2 will not be able to deliver 5 V since the undervoltage lockout of the secondary side is set at 12 V. Hence minimum the recommended output voltage is around 15 V.

2EDF7275F is a 4 V -versions for logic-level MOSFETs and only this driver can deliver 5 V at 2 A continuous on each output.
0 Likes