Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User22451
Level 1
Level 1
Dear Community,

Hi, to all
I want to test desat pin function without any kind circuit?
Is there any approach for test only fault section without connecting igbt/mosfet to it?
0 Likes
1 Solution
Abhilash_P
Moderator
Moderator
Moderator
50 likes received 500 replies posted 250 solutions authored
Hi,

The desat pin of 1ed family can be tested as follows,
" For this testing the desat pin external circuit (cap, resistor and diode) is still required. If you give an ON signal to the driver and reverse bias that DESAT diode, the constant current source will will eventually charge up the desat capacitor and trigger DESAT protection. This step is similar to the case that when a short circuit is happening and the Vce(sat) is too high and not able to clamp (bring down) the desat pin voltage."


Regards,
Abhilash P

View solution in original post

0 Likes
3 Replies
Abhilash_P
Moderator
Moderator
Moderator
50 likes received 500 replies posted 250 solutions authored
Hi,

The desat pin of 1ed family can be tested as follows,
" For this testing the desat pin external circuit (cap, resistor and diode) is still required. If you give an ON signal to the driver and reverse bias that DESAT diode, the constant current source will will eventually charge up the desat capacitor and trigger DESAT protection. This step is similar to the case that when a short circuit is happening and the Vce(sat) is too high and not able to clamp (bring down) the desat pin voltage."


Regards,
Abhilash P
0 Likes
User22451
Level 1
Level 1
hey,
Thanks, Abhilash P for the reply. I have another doubt about which type of cap we have to use electrolyte, ceramic, or titanium.
0 Likes
Abhilash_P
Moderator
Moderator
Moderator
50 likes received 500 replies posted 250 solutions authored
Hi,

It can only be a ceramic capacitor. This is because the range of capacitance for this is in several hundreds pF.

Regards,
Abhilash P
0 Likes