Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Gate Driver ICs Forum Discussions

User16966
Level 1
Level 1
Hello All,

I'm using IGCM20F60GA as three phase driver.
in the data sheet is not reported the minimum ON time of this module.
I mean what is the minimum pwm ON time I can apply to the driver without damaging it?
Thanks
Andrea
0 Likes
1 Solution
AZIZ_HASSAN
Moderator
Moderator
Moderator
25 likes received 100 sign-ins 50 solutions authored

Hi,

As stated in the above comment attachment, the minimum On time of pulse should be  290nsec.

 

BR,

AZIZ HASSAN

View solution in original post

0 Likes
2 Replies
Emanuel
Employee
Employee
10 solutions authored 5 solutions authored First solution authored
hi AndreaC,

Generally, a too short pulse cannot damage the driver IC, but it will not be propagated to the output (the signal will not be registered).
Some gate driver (including the one in the IGCM20F60GA) have an input filter. This is to ensure that unintended spikes (due to parasitic coupling) are not triggering the gate driver.
In the case of this product, the input filter is around 290 ns (see table at page 10).
3978.attach
0 Likes
AZIZ_HASSAN
Moderator
Moderator
Moderator
25 likes received 100 sign-ins 50 solutions authored

Hi,

As stated in the above comment attachment, the minimum On time of pulse should be  290nsec.

 

BR,

AZIZ HASSAN

0 Likes