Employee
Yuyan_Tang
Employee
Nov 13, 2017
06:56 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
The bootstrap power supply is one of the most widely used methods to supply power to the high-side drive circuitry of a gate driver IC. It consists of a bootstrap diode and a bootstrap capacitor as shown in the following figure.

This method has the advantage of being both simple and low-cost. However, the requirement to refresh the charge on the bootstrap capacitor may result in limitations on the power converter’s duty-cycle and power switch’s on-time. Proper capacitor and bootstrap resistance selection can drastically reduce these limitations. For more information, please refer to the following two application notes:
https://www.infineon.com/dgdl/Infineon-Using+Monolithci+Voltage+Gate+Drivers-UM-v01_00-EN.pdf?fileId...
https://www.infineon.com/dgdl/an-978.pdf?fileId=5546d462533600a40153559f7cf21200
This method has the advantage of being both simple and low-cost. However, the requirement to refresh the charge on the bootstrap capacitor may result in limitations on the power converter’s duty-cycle and power switch’s on-time. Proper capacitor and bootstrap resistance selection can drastically reduce these limitations. For more information, please refer to the following two application notes:
https://www.infineon.com/dgdl/Infineon-Using+Monolithci+Voltage+Gate+Drivers-UM-v01_00-EN.pdf?fileId...
https://www.infineon.com/dgdl/an-978.pdf?fileId=5546d462533600a40153559f7cf21200
- Tags:
- IFX
0 Replies