#IR2113E6の内部回路について確認したいです.

(1) Regarding the digital side and the drive side, is it correct to assume that the GND line is isolated inside the device?

(2) Due to the specifications of the peripheral circuit, are there any problems when the GND of the digital side and the analog side are common?

(3) Also, when a voltage of 375 V is applied between VB and COM and 360 V between VS and COM, will current flow occur when the voltage between VB and VS becomes about 15 V → 1 V?

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E3%82%B2%E3%83%BC%E3%83%88%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BCIC/IR2113E6%E3%81%AE%E5%86%85%E9%83%A8%E5%9B%9E%E8%B7%AF%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6/td-p/665141

0 Likes
1 Solution
Translation_Bot
Community Manager
Community Manager
Community Manager

Dear MOTOKI ,

 

Thank you for using our service.

 

>> (1) Is it correct to assume that the GND line is isolated inside the device for the digital side and the drive side?

No. It is not an isolated driver.

 

>> (2) Is there any problem when the GND of the digital side and the analog side are shared due to the specifications of the peripheral circuit?

There is no problem with connecting DGND and AGND to determine the potential. However, depending on the actual pattern design, there is a possibility that unexpected surges will occur. We hope that you will pay close attention to the current path when designing the pattern.

 

>> (3) Also, when a voltage of 375 V is applied between VB and COM and 360 V between VS and COM, will current flow occur when the voltage between VB and VS becomes about 15 V → 1 V?

In the case of a half-bridge, the voltage charging of the capacitor is performed in the process of turning on the low-side power device. I don't know the customer's specifications, but if the high-side capacitor falls below the threshold value of the high-side gate, the high-side power device will be turned off and the discharge will be stopped. If the power device is an IGBT, the discharge should generally stop before it reaches 1V.

 

European

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E3%82%B2%E3%83%BC%E3%83%88%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BCIC/IR2113E6%E3%81%AE%E5%86%85%E9%83%A8%E5%9B%9E%E8%B7%AF%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6/m-p/672805

View solution in original post

0 Likes
6 Replies
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello.
Appreciate your contact regarding this matter.
Rest assured, diligent review of the provided contents is underway. The aim is to provide a comprehensive response soon.
Your understanding and patience are sincerely appreciated.

Best regards,
Tengfei

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E3%82%B2%E3%83%BC%E3%83%88%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BCIC/IR2113E6%E3%81%AE%E5%86%85%E9%83%A8%E5%9B%9E%E8%B7%AF%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6/m-p/668563

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

Dear MOTOKI ,

 

Thank you for using our service.

 

>> (1) Is it correct to assume that the GND line is isolated inside the device for the digital side and the drive side?

No. It is not an isolated driver.

 

>> (2) Is there any problem when the GND of the digital side and the analog side are shared due to the specifications of the peripheral circuit?

There is no problem with connecting DGND and AGND to determine the potential. However, depending on the actual pattern design, there is a possibility that unexpected surges will occur. We hope that you will pay close attention to the current path when designing the pattern.

 

>> (3) Also, when a voltage of 375 V is applied between VB and COM and 360 V between VS and COM, will current flow occur when the voltage between VB and VS becomes about 15 V → 1 V?

In the case of a half-bridge, the voltage charging of the capacitor is performed in the process of turning on the low-side power device. I don't know the customer's specifications, but if the high-side capacitor falls below the threshold value of the high-side gate, the high-side power device will be turned off and the discharge will be stopped. If the power device is an IGBT, the discharge should generally stop before it reaches 1V.

 

European

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E3%82%B2%E3%83%BC%E3%83%88%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BCIC/IR2113E6%E3%81%AE%E5%86%85%E9%83%A8%E5%9B%9E%E8%B7%AF%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6/m-p/672805

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

Thank you for contacting us.

I would like to explain a specific example, but it is difficult to present detailed information in an open place, so is it possible to contact them directly?

In fact, the internal circuit of the device IR2113E6 is burned out in the usage environment, and it is difficult to know the cause.

Thank you for your consideration.

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E3%82%B2%E3%83%BC%E3%83%88%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BCIC/IR2113E6%E3%81%AE%E5%86%85%E9%83%A8%E5%9B%9E%E8%B7%AF%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6/m-p/672821

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

Dear MOTOKI,

If necessary, create a case from Mycase in myinfineon.

Tengfei_O_0-1704776678855.png

Thank you.

European

 

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E3%82%B2%E3%83%BC%E3%83%88%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BCIC/IR2113E6%E3%81%AE%E5%86%85%E9%83%A8%E5%9B%9E%E8%B7%AF%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6/m-p/672839

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

I have put it in MyCASE, so please check it.

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E3%82%B2%E3%83%BC%E3%83%88%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BCIC/IR2113E6%E3%81%AE%E5%86%85%E9%83%A8%E5%9B%9E%E8%B7%AF%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6/m-p/673099

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

(2) The primary and secondary GNDs must not be the same. If this is the case, the high-side voltage will be applied to the internal element of the low breakdown voltage, and it will be destroyed.

 

As mentioned above, VSS and COM are common in the circuit for measuring specifications in the data sheet, so I wonder if the data sheet is correct in the above opinion. Isn't VDD and VCC common, not GND?

Please check it.

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E3%82%B2%E3%83%BC%E3%83%88%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BCIC/IR2113E6%E3%81%AE%E5%86%85%E9%83%A8%E5%9B%9E%E8%B7%AF%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6/m-p/674963

0 Likes