公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
ZhangLi1
Level 1
Level 1
5 questions asked First like given 5 replies posted

你好,我想请问一下
我在应用手册中看到了对于DESAT引脚保护二极管的一段描述

ZhangLi1_0-1673760565172.png

描述中提到了“不允许低于-0.3V”,但没有具体指出是哪个参数不允许低于-0.3V。我猜测是导通压降不允许低于0.3V?
请问我猜测的正确吗?谢谢!

0 点赞
1 解答
Alex_S
Level 2
Level 2
First solution authored 10 replies posted 10 sign-ins

Hi,

if my translation of your question is correct, you would like to know which parameter is limited to "-0.3V", the voltage on the "DESAT"-Pin (referenced to GND2) is not allowed to be lower than "-0.3V". Please have a look on page 18 in the datasheet "Absolute maximum ratings => DESAT voltage". Hope this helps.

 

BR

Alex

在原帖中查看解决方案

0 点赞
4 回复数
Alex_S
Level 2
Level 2
First solution authored 10 replies posted 10 sign-ins

Hi,

if my translation of your question is correct, you would like to know which parameter is limited to "-0.3V", the voltage on the "DESAT"-Pin (referenced to GND2) is not allowed to be lower than "-0.3V". Please have a look on page 18 in the datasheet "Absolute maximum ratings => DESAT voltage". Hope this helps.

 

BR

Alex

0 点赞
ZhangLi1
Level 1
Level 1
5 questions asked First like given 5 replies posted

我按照你说的去查看一下手册!感谢你的回答!

0 点赞
Rachel_G
Moderator
Moderator
Moderator
50 likes received 250 solutions authored 250 replies posted

Hi  

根据datasheet的参数表, 1ED3322MC12N 的Desat pin的最大额定值范围在-0.3V到Vcc2+0.3V之间(参考GND2),所以选择的保护二极管的正向导通压降的绝对值不应高于0.3V。

Best regards,

Rachel

0 点赞
ZhangLi1
Level 1
Level 1
5 questions asked First like given 5 replies posted

感谢你的回答!这解决了燃眉之急!

0 点赞