Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

GaN Forum Discussions

Translation_Bot
GaN
Hello, I would like to purchase GaN HEMT for use in electric vehicle drives. May I know which model is suitable? Thank you very much!smartconx_target@... Show More
Translation_Bot
GaN
Hello, I made an inverter, input 150V DC, switching frequency 200kHz, modulation ratio 0.7, load 100 ohms. IGI60F1414A1L is used, and the peripheral c... Show More
Benjamin_han
GaN
My question is, can I use Ansyssimplorer software to model the GaN HEMT model? Modeling requires simulation in an inverter driven by a motor, and then... Show More
Translation_Bot
GaN
Hi Experts, Recently I was evaluating the dynamic performance of GaN MOS, the device model is GS-065-030. while doing the double pulse test, I found t... Show More
pramod_p1
GaN

I have ordered a GAN Daughter Card (GS66508T), Can Anyone confirm whether it is Gate Driver only or Gate Driver Plus GAN switches?

Manex
GaN
Hi, I’m designing a 7 kW converter in which each switch conducts 30 A RMS. However, when I analyze the Safe Operating Area (SOA) of the IGOT60R042D1 M... Show More
Translation_Bot
GaN
Does GaN mosfet not have this device? I need to purchase a gallium nitride chip to be placed in a motor driven inverter. Before doing so, I need to co... Show More
PremaPerumal
GaN
Gan FET
solved msg Solved
We are planning to use High current Gan FET Below mentioned our requirement follow this, 1. DC continuous 150A and Above 2.VDS=150V and above 2.VGS = ... Show More
Rafa
GaN
Hi, There is an evaluation board for the IGI60F1414A1L GaN half bridge but its not possible to buy. I was wondering if you could share the so called e... Show More
avtjonesyu
GaN
Hello team,   Hope you are doing well!   My customer is looking for an integrated power stage with Vds=100V, 15A/25A/35A, Rds(On)<10mΩ. So it’s a half... Show More
Forum Information

GaN

Infineon offers highly efficient GaN (gallium nitride) transistor-based industry leading Gate Injection Transistor (GIT) technology and Schottky Gate technology. With the acquisition of GaN systems Infineon's CoolGaN™ offers GaN from 100V to 700V range, these products have fast turn-on/-off speed, minimum switching losses, and a large variety of package options, enabling simple and fast time-to-market. In addition, Infineon also offers GaN (single switch and half bridge configuration) with integrated gate driver, current sense, and various protections. These integrated GaN could be driven from a digital PWM input, allows short dead-time setting to maximize system efficiency and available in small package for compact system designs. Infineon's CoolGaN™ and Integrated GaN are most viable option in different applications like USB-C adapters and chargers, 48 V power distribution, server and telecom SMPS, solar and energy storage systems, motor drives, robots and drones, and more. In this forum, you can post your questions, comments, and feedback about GaN devices and their applications.