Announcements

Live Webinar: Solving the challenges in xEV power conversions | March 7 @9am & 5pm CET. Register now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

GaN Forum Discussions

Sort by:
e2s
GaN
Hi community, we have a 1.5KW LLC application. The switching frequency is 1MHz. The input voltage is 400V DC, the output voltage unregulated approx. 1... Show More
mtburche
GaN
Hello, I would like any available documentation with the installed component values on the GaN Systems GSWP300W-EVBPA development board -- the Technic... Show More
cabesamis
GaN
P/N GS61004B What are the outgoing inspections performed for the above part number? 100% electrical and visual? Thank you.
cabesamis
GaN
P/N GS61004B What is the ESD rating and Moisture Level (MSL) for the above part number?
antonypeter
GaN
GanFET
solved msg Solved

From when onwards GanFET with 900V or 1200V will be available. Any idea?

GeYou-bit
GaN
      我正在搭建一个电机实验平台,现在已经有电机(PMSM)和控制器(DSP2835),缺少电机驱动板,希望大家能推荐给我几款电机驱动板,非常感谢。 电机参数: 额定电压AC220,依据SVPWM原理换算成直流为311V 额定功率1.5KW 额定电流6.5A,瞬时峰值电流可以达到13A Show More
joynag
GaN
Hello everyone, I am using 1EDN7116UXTSA1 gate driver in my design. During the preliminary testing, the low side gate driver gets super hot (draws 600... Show More
lixuancheng
GaN
The drive waveform of IGT60R070D1 starts to exhibit jitter as the load increases. What could be the cause? 50 Ohm load:   100 Ohm load:     Show More
YuTa_4942221
GaN
Let me confirm one point regarding EVAL_2EDB_HB_GAN.Is it possible to provide electronic data regarding the schematic, layout (silk), and BOM listed o... Show More
Kelly_Yu
GaN
As we known,There are Two types of GaN hemt,one is  GIT,the other is SG,so,how can I confirm which type of the device choose from datasheet. THX SOOO ... Show More
Forum Information

GaN

Infineon’s CoolGaN™ is a highly efficient GaN (gallium nitride) transistor technology for power conversion in the voltage range up to 600V. The pioneering quality ensures the highest standards and offers the most reliable and performing solution among all GaN HEMTs on the market. Switched-mode power circuits using CoolGaN™ can benefit from the improved energy efficiency and the improved power density, which is not possible with state-of-the-art silicon devices. In this forum, you can post your questions, comments, and feedback about CoolGaN™ devices and their applications.