Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Forums Forum Discussions

Browse the Community

USB

Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.

61499701 11582

Memories

Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.

10401656 2770

Other Technologies

Discussion forum regarding Other Technologies including Power Management and Clocks topics.

1148749 799

Software

Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .

94271297 15196
filter icon

Featured Discussions

Sort by:
ccitxue
Motor Control ICs

在应用MCE Designer 跟踪功能调试速度环参数时,由于我们电机额定速度只有340rpm,而跟踪虚拟示波器的X轴量程又不能设置超过512,导致在速度从100rpm加速到额定值340rpm时看不到速度动态变化图形,请问如何解决?

kdunahee
AURIX™

Does AURIX(TM) Development Studio support development of SCR including C toolchain and debugging?

RLGeorge
MOTIX™ MCU
I need to enable password protection for NVM Code Protection. I see in Config Wizard, SCU where the code protection can be enabled and a pass word sel... Show More
user_4495571
PSoC™ 5, 3 & 1

Hi,

for my UART port pins there is no API generated.

Under Mapping Contiguous is selected.

Whats going on?

Yalcin_Haksoz
XMC™
Hi, I am trying to get the FPU going on XMC4200 but for some reason I am not able to get the expected performance. I am using the latest version of DA... Show More
GarageDirt
XMC™
I have two analog signals in the shape of a gaussian curve having an amplitude of about 500 mv and duration of 20 microseconds.  These pulses happen a... Show More
Parallels_User
PSoC™ 4
Has anyone had success programming a CY8CKIT-042-BLE-A on Windows 11 ARM running in Parallels on an M1/M2 Mac? It shows up in the device manager as no... Show More
Diesel999
PSoC™ 4
Still looking for a person who can help with a client program for my product. see vyndicator.com. Looked at a few suggested programs from the 100 day ... Show More
mok_2000
PSoC™ 4
I am running ModusTool Box on Linux. While it is running ok, it does not show my particular development board which belongs to the PSoC 4200 series. A... Show More
Komugiz_King
PSoC™ 6
  Hello everyone, I'd like to discuss a modification I'm currently working on for the CY8C6347BZI-BLD53 board, using the example code CE220924. This ... Show More