Diodes & Thyristors (Si/SiC) Forum Discussions
SiC Schottky diode: I have a question about IDD05SG60C.
From the description of the following material, it is said that reflow can be done up to 3 times on the preconditioning test,
How many times can it actually be reflowed?
Also, if I reflow at 160°C below 260°C, will it be counted as the number of times?
Product Qualification Report
IDD05SG60C
Show LessI am searching for new old or a suggestion for a substitute part for a Bauer 707 broadcast transmitter silicon rectifier that was made at International Rectifier Corp the part number is 67-6288 U5. I figure this is along shot but why not try this avenue. I believe one or both are toast and there is not a way for me to test them but everything is pointed to this as the bad part in troubleshooting.
Show LessHello,
I'm trying to simulate transient behavior of four IDDD08G65C6 diodes.
I downloaded the model "Infineon-SimulationModel_SiC_Diodes_CoolSiC_PSpice_Generation6_DDPAK.-SM-v01_00-EN" and added the library "SimulationModel_PSpice_G6_650V_DDPAK" to my design by associating "IDDD08G65C6 _L3" model to a part.
When I launch simulation, PSpice made errors as shown below.
In the Simulation setting-- Configuration files -- Library, I have tried to add "diode.lib" as global or to design. But this doesn't fix the problem.
I also tried to add "Zener.lib" "Infineon.lib" "dual_diode.lib" "analog.lib" "diode_fullbridge.lib" "breakout.lib" to design, but those cannot fix the problem.
I am using Orcad PSpice V17.4.2019
Can someone help me?
Show LessPlease tell me one thing about DD750S65K3 /DD1200S45KL3_B5.
There is a definition of VRRM in the data sheet, but how should we think about VRSM?
Even in the case of VRSM-like operation, will it be possible to keep it within the VRRM value?
・型番DD750S65K3 /DD1200S45KL3_B5
Show Less
Hello
Does Infineon have any solution for IEC-1000-4-6 (not IEC 1000-4-5)) who applies RF (150K~8M)stress
which is current injection ?
Customer says TVS is not valid for this ( current- type noise), and customer's product is small for using Big-size
choke coil...
Please advise.
Thank you for your cooperation
Show Less
Need alternate for MPN IRFR120NTRPBF
Does anyone have the pinout for the STT series of Soft Start Modules (e.g. STT1900N16P55)? It seems to be missing from the data sheet.
Also, is there a recommended mounting method for this device?
Thanks.
~LMG
Show Less
Let me confirm one point about the flat Diode.
In the datasheet, the surge current is IFSM=110,000A.
Would it be okay to extrapolate the Vf-If characteristics when that current flows, as shown in the attached Excel sheet?
We apologize for the inconvenience, but please confirm.
Show Less英飞凌的快速开关型晶体管中能满足一下条件的有哪些型号? (1)工作电流(或漏源电流)致少大于4A, (2)触发脉冲辐度:低于2-3V; (3)工作电压:大于25v (4)工作频率:大于800MHZ 芯片在脉冲工作时的上升、下降沿一般在2-4ns量级