Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

DAVE™ Forum Discussions

mgritz
DAVE™
There's a bug in the DAVE-generated EEPROM emulation driver for the XMC4800, working with DAVE v4.5 and the E_EEPROM_XMC4 App v4.0.20. In Dave/Generat... Show More
Azzo
DAVE™
Hi everyone, The PWM App does not allow CCU8 to be selected in DAVE 4.3.2 although the App Help states that CCU8 is an option. Is this just a document... Show More
µCGuru334
DAVE™
Hello. How can i solve the problem with the SPI-MASTER App with a XMC4700 microcontroller. I use the SPI_MASTER App and select "Enable advanved pin co... Show More
Tarun_M
DAVE™
Hello,I am using the ADC and UART peripherals of XMC4400 Board. I am trying to read the sensor values using the ADC. And, next, I wish to check the re... Show More
Azzo
DAVE™
Hi everyone, I am running DAVE v4.3.2 and the 'ENCODER_POSIF' APP is missing. If I check for DAVE APP updates the 'ENCODER_POSIF' does not appear in ... Show More
Azzo
DAVE™
Hi all, Would anyone know the purpose of the 't_offset' parameter in the following function please ?  It is not documented the v4.0.6 App help.     EN... Show More
Azzo
DAVE™
Hi All, I have a project with 3 x PWM Apps using 3 x CCU4's. When I add the ENCODER_POSIF App and I select 'New App Instance' to use the 4th CCU4 I ge... Show More
NXTY_hayashi
DAVE™
Hi, DAVE App of EVENT_GENERATOR for ERU has only single "pattern" input, it has no "tout" output.XMC1400 ERU has 4 inputs EXICONx.FL to detect pattern... Show More
Imperius
DAVE™
Hi,   I have an IMU which uses I2C for configuration. The device uses only one byte writing, meaning that the master may transmit only one byte of dat... Show More
User17806
DAVE™
Hi,I need two external interrupt in my project and want to use BUTTON1 (P1.14) and BUTTON2 (P1.15) on xmc4500 Relax Kit. I added PIN_INTERRUPT App to ... Show More