DAVE™ Forum Discussions
DAVE™
Hello 🙂I have a question to the SYSTM002 App parameter in DAVE 3. The first and second parameter are clearly, but i didnt't understand the third. I t...
Show More
Hello 🙂
I have a question to the SYSTM002 App parameter in DAVE 3. The first and second parameter are clearly, but i didnt't understand the third. I tried it with a method, nevertheless i don't understand.
In my code i have a line like this:
SYSTM002_CreateTimer(1000, SYSTM002_ONE_SHOT, ???, NULL);
Can somebody explain me the third parameter? This would be very helpful. 🙂
Many thanks in advance! Show Less
I have a question to the SYSTM002 App parameter in DAVE 3. The first and second parameter are clearly, but i didnt't understand the third. I tried it with a method, nevertheless i don't understand.
In my code i have a line like this:
SYSTM002_CreateTimer(1000, SYSTM002_ONE_SHOT, ???, NULL);
Can somebody explain me the third parameter? This would be very helpful. 🙂
Many thanks in advance! Show Less
DAVE™
Hi everybody, I'm using Dave 4.1. I was adding Apps in my project, when I got thi error: "Dave is not able to grant your last hardware resources reque...
Show More
Hi everybody,
I'm using Dave 4.1. I was adding Apps in my project, when I got thi error: "Dave is not able to grant your last hardware resources request".
Does anybody ever dealt with this problem?
Thanks in advance for any advice.
Best regards,
Andrea. Show Less
I'm using Dave 4.1. I was adding Apps in my project, when I got thi error: "Dave is not able to grant your last hardware resources request".
Does anybody ever dealt with this problem?
Thanks in advance for any advice.
Best regards,
Andrea. Show Less
DAVE™
Dear Members,I tried many times to generate the codes according to BLDC example in Dave 3 and faced problems as attached file. The warnings are "Resou...
Show More
Dear Members,
I tried many times to generate the codes according to BLDC example in Dave 3 and faced problems as attached file. The warnings are "Resource mapping failed, please review the user defined constraints" and "Solver failed to execute, code generation cannot be started." Could you please show me a solution for these problems?
Best Regards
Erkan Eren Show Less
I tried many times to generate the codes according to BLDC example in Dave 3 and faced problems as attached file. The warnings are "Resource mapping failed, please review the user defined constraints" and "Solver failed to execute, code generation cannot be started." Could you please show me a solution for these problems?
Best Regards
Erkan Eren Show Less
DAVE™
Hello,I'm using two instances of the HRPWM-App and want to use them to control a Full Bridge with Phase Shift as shown on pages 16 to 18 in the traini...
Show More
Hello,
I'm using two instances of the HRPWM-App and want to use them to control a Full Bridge with Phase Shift as shown on pages 16 to 18 in the training file (http://www.infineon.com/dgdl/Infineon-IP_HRPWM_XMC4-TR-v01_01-EN.pdf?fileId=5546d4624ad04ef9014b0780db972267). Therefor I tried to connect the event_ch2_cmp_match signal of instance one to the hrc_set0 signal of instance 2. Unfortunately this doesn't work out as Dave doesn't provide this connection possibility in the HW signal connection window. Can anyone help me or give me a hint, what I'm doing wrong?
Best regards,
Markus Show Less
I'm using two instances of the HRPWM-App and want to use them to control a Full Bridge with Phase Shift as shown on pages 16 to 18 in the training file (http://www.infineon.com/dgdl/Infineon-IP_HRPWM_XMC4-TR-v01_01-EN.pdf?fileId=5546d4624ad04ef9014b0780db972267). Therefor I tried to connect the event_ch2_cmp_match signal of instance one to the hrc_set0 signal of instance 2. Unfortunately this doesn't work out as Dave doesn't provide this connection possibility in the HW signal connection window. Can anyone help me or give me a hint, what I'm doing wrong?
Best regards,
Markus Show Less
DAVE™
Hi sir:
How to use DAVE to combine PWM_BC with POSIF in APP project ?
How to use DAVE to combine PWM_BC with POSIF in APP project ?
DAVE™
hi,after upgrade to DAVE 4.2.2 and install LWIP, i get an "Generate Code" error : in "File "ethernetif.tcmp""Cannot invoke method toInteger() on null ...
Show More
hi,
after upgrade to DAVE 4.2.2 and install LWIP, i get an "Generate Code" error : in "File "ethernetif.tcmp"
"Cannot invoke method toInteger() on null object ethernetifc.tmpl /LWIP_TEST/Dave/Model/APPS/ETH_LWIP/v4_0_4/Templates line 498 Groovy Template"
out.print("""
port_control.clk_rmii = (XMC_ETH_MAC_PORT_CTRL_CLK_RMII_t)${eth_lwip_inst.hwres_eth_mac.getRegValue("con","con_rmii").toInteger()}U;
attached is the (XMC4700) DAVE CE Project.
Regards,
Torsten Show Less
after upgrade to DAVE 4.2.2 and install LWIP, i get an "Generate Code" error : in "File "ethernetif.tcmp"
"Cannot invoke method toInteger() on null object ethernetifc.tmpl /LWIP_TEST/Dave/Model/APPS/ETH_LWIP/v4_0_4/Templates line 498 Groovy Template"
out.print("""
port_control.clk_rmii = (XMC_ETH_MAC_PORT_CTRL_CLK_RMII_t)${eth_lwip_inst.hwres_eth_mac.getRegValue("con","con_rmii").toInteger()}U;
attached is the (XMC4700) DAVE CE Project.
Regards,
Torsten Show Less
DAVE™
I have been working a lot with DAVE3.1.10 and was quite pleased. It's now time to start a new development project, and installed the new DAVE4 IDE. Wi...
Show More
I have been working a lot with DAVE3.1.10 and was quite pleased.
It's now time to start a new development project, and installed the new DAVE4 IDE. Will use FreeRTOS so i thought DAVE4 to be an upgrade since i now have it implemented as an app - great!
I was intending to measure dutycylce on an digital input. My question is: How do i achieve this in DAVE4 when CAP001 is left out? Show Less
It's now time to start a new development project, and installed the new DAVE4 IDE. Will use FreeRTOS so i thought DAVE4 to be an upgrade since i now have it implemented as an app - great!
I was intending to measure dutycylce on an digital input. My question is: How do i achieve this in DAVE4 when CAP001 is left out? Show Less
DAVE™
Hi,I'm trying to create a simple TCP socket server using Dave App ETH_LWIP.LwIP is correctly running and I'm able to ping my board.Can you suggest me ...
Show More
Hi,
I'm trying to create a simple TCP socket server using Dave App ETH_LWIP.
LwIP is correctly running and I'm able to ping my board.
Can you suggest me some documents? I don't undestand which "methods" I can use. Do I have to include some header files in the main file?
Thank you
Regards
Matteo Show Less
I'm trying to create a simple TCP socket server using Dave App ETH_LWIP.
LwIP is correctly running and I'm able to ping my board.
Can you suggest me some documents? I don't undestand which "methods" I can use. Do I have to include some header files in the main file?
Thank you
Regards
Matteo Show Less
DAVE™
Hi everybody, I'm a very beginner with Dave. I'm Using Dave 3.1.10 with an XMC 4500. The problem is that I can't add new Apps into an existing project...
Show More
Hi everybody,
I'm a very beginner with Dave. I'm Using Dave 3.1.10 with an XMC 4500.
The problem is that I can't add new Apps into an existing project which already contains applications.
I checked path settings and if libraries are installed. Everything seems to be ok,but the App Selection View is empty.
Can anybody help me with this trouble?
Thanks in advance for any advice.
Best regards,
Andrea. Show Less
I'm a very beginner with Dave. I'm Using Dave 3.1.10 with an XMC 4500.
The problem is that I can't add new Apps into an existing project which already contains applications.
I checked path settings and if libraries are installed. Everything seems to be ok,but the App Selection View is empty.
Can anybody help me with this trouble?
Thanks in advance for any advice.
Best regards,
Andrea. Show Less