DAVE™ Forum Discussions
DAVE™
I use DAVE™ (Version 4) for XMC4500 and the peripheral ETH0.In the XMC Lib in the file xmc_eth_mac.c there is an assert (l. 328 and l. 408), which see...
Show More
I use DAVE™ (Version 4) for XMC4500 and the peripheral ETH0.
In the XMC Lib in the file xmc_eth_mac.c there is an assert (l. 328 and l. 408), which seem strange to me:
XMC_ASSERT("XMC_ETH_MAC_SendFrame:", eth_mac->regs != ETH0);
Why should the eth_mac->regs not be ETH0?
My Application, that works well, always gets stuck in this assert.
Does it mean something? Show Less
In the XMC Lib in the file xmc_eth_mac.c there is an assert (l. 328 and l. 408), which seem strange to me:
XMC_ASSERT("XMC_ETH_MAC_SendFrame:", eth_mac->regs != ETH0);
Why should the eth_mac->regs not be ETH0?
My Application, that works well, always gets stuck in this assert.
Does it mean something? Show Less
DAVE™
Hello everybody,im trying to debug and program a XMC4500 via Dave 4, since I don't own a windows PC i try it via a vm on my Macbook. The problem now i...
Show More
Hello everybody,
im trying to debug and program a XMC4500 via Dave 4, since I don't own a windows PC i try it via a vm on my Macbook.
The problem now is that I get a gdb timeout error(see screenshot).
What i've tried so far:
Maybe someone also had this problem in the past and knows a solution or has a good hint how to solve the problem.
Kind regards,
Pascal
Show Less
im trying to debug and program a XMC4500 via Dave 4, since I don't own a windows PC i try it via a vm on my Macbook.
The problem now is that I get a gdb timeout error(see screenshot).
What i've tried so far:
- reconnect the XMC4500 and make sure the XMC is connected to the VM and not the Mac
- switched off both firewalls
- tried to program the XMC4500 via remote connection to the host machine(the Mac)
Maybe someone also had this problem in the past and knows a solution or has a good hint how to solve the problem.
Kind regards,
Pascal
Show Less
DAVE™
can anyone help me to use this function Get_Time in app SYSTM001, i want to make project with HC-SR04 ultrasonic ranging module with DAVE 3 and XMC 45...
Show More
can anyone help me to use this function Get_Time in app SYSTM001, i want to make project with HC-SR04 ultrasonic ranging module with DAVE 3 and XMC 4500 Relax Lite Kit, but i can't get time in ms to know distance with some object.
thanks Show Less
thanks Show Less
DAVE™
The I2C_MASTER app seems to be totally unable to handle an unexpected NACK. It just loops forever waiting for an ACK. What can I do?
Randy
Randy
DAVE™
What for Debugger can I use in DAVE except J-Link? I have a Ulink2 already. Is it possible to integrate this device in DAVE?I don't need JTAG, for SWD...
Show More
What for Debugger can I use in DAVE except J-Link?
I have a Ulink2 already. Is it possible to integrate this device in DAVE?
I don't need JTAG, for SWD only. Show Less
I have a Ulink2 already. Is it possible to integrate this device in DAVE?
I don't need JTAG, for SWD only. Show Less
DAVE™
Good old 16550 uart device had a fifo timeout interrupt.If you use f.e. 16 bytes fifo as a uart receive buffer and set the receive trigger to about 10...
Show More
Good old 16550 uart device had a fifo timeout interrupt.
If you use f.e. 16 bytes fifo as a uart receive buffer and set the receive trigger to about 10,
how will you get an interrupt when only one byte arrives ? Show Less
If you use f.e. 16 bytes fifo as a uart receive buffer and set the receive trigger to about 10,
how will you get an interrupt when only one byte arrives ? Show Less
DAVE™
Hi Guys,I'm trying out some of the new Apps released with Dave 4.2.4.In fact I'm using a XMC4800 F144-2048 and a XMC4500 F144-1024I set up the new ETH...
Show More
Hi Guys,
I'm trying out some of the new Apps released with Dave 4.2.4.
In fact I'm using a XMC4800 F144-2048 and a XMC4500 F144-1024
I set up the new ETH_LWIP App for both chips in the RAW variant (without any operating system).
With the '45 it works pretty fine. The '48 throws an error during the code generation:
The referenced line is the following:
From the first glance I would guess, that there is an error within the Hardware Describtion File.
But before submitting a ticket, I would like to ask, if anyone is able to reproduce this bug.
If additional informations are needed just ask.
Cheers Tobi Show Less
I'm trying out some of the new Apps released with Dave 4.2.4.
In fact I'm using a XMC4800 F144-2048 and a XMC4500 F144-1024
I set up the new ETH_LWIP App for both chips in the RAW variant (without any operating system).
With the '45 it works pretty fine. The '48 throws an error during the code generation:
Cannot invoke method toInteger() on null object ethernetifc.tmpl /test/Dave/Model/APPS/ETH_LWIP/v4_0_4/Templates line 498 Groovy Template
The referenced line is the following:
port_control.clk_rmii = (XMC_ETH_MAC_PORT_CTRL_CLK_RMII_t)${eth_lwip_inst.hwres_eth_mac.getRegValue("con","con_rmii").toInteger()}U;
From the first glance I would guess, that there is an error within the Hardware Describtion File.
But before submitting a ticket, I would like to ask, if anyone is able to reproduce this bug.
If additional informations are needed just ask.
Cheers Tobi Show Less
DAVE™
HI,I want to use the PWM (PWMSP001 ) on XMC1100 but when I try to generate the code it's says "Fail to update one or more resources".I tried to update...
Show More
HI,
I want to use the PWM (PWMSP001 ) on XMC1100 but when I try to generate the code it's says "Fail to update one or more resources".
I tried to update all XMC1100 files as you mention on this forum for this type of error but no succes.
I seen there was another post where the same problem was mentioned.
I have to stick with DAVE3.
Is there any solution?
Thank you. Show Less
I want to use the PWM (PWMSP001 ) on XMC1100 but when I try to generate the code it's says "Fail to update one or more resources".
I tried to update all XMC1100 files as you mention on this forum for this type of error but no succes.
I seen there was another post where the same problem was mentioned.
I have to stick with DAVE3.
Is there any solution?
Thank you. Show Less
DAVE™
HiThedocument: Infineon-TOOL_Tutorial_DAVE_genCode_to_Atollic_XMC-TR-v01_00-EN.pdffrom website: http://www.infineon.com/cms/en/product/microcontroller/32-bit-industrial-microcontroller-based-on-arm-registered-cortex-register...
Show More
Hi
Thedocument: Infineon-TOOL_Tutorial_DAVE_genCode_to_Atollic_XMC-TR-v01_00-EN.pdf
from website: http://www.infineon.com/cms/en/product/microcontroller/32-bit-industrial-microcontroller-based-on-arm-registered-cortex-register
has an error.
regards
zbyno Show Less
Thedocument: Infineon-TOOL_Tutorial_DAVE_genCode_to_Atollic_XMC-TR-v01_00-EN.pdf
from website: http://www.infineon.com/cms/en/product/microcontroller/32-bit-industrial-microcontroller-based-on-arm-registered-cortex-register
has an error.
regards
zbyno Show Less