Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

DAVE™ Forum Discussions

Sort by:
MaxECU
DAVE™
Looking at the System Timer application, I do not find any App that could provide a simple Delay_usec(uint32_t uiUs) function? Is there any possibilit... Show More
User17265
DAVE™
Hi.I would like to know if there is a way to control the initialization order of DAVE APPs in *autogenerated* DAVE_Init().My concern is* in autogenera... Show More
User12713
DAVE™
Hello,Could I make program SPI running in background? For example 4 SPI groups (x3 channels) and these channels work in Background. (XMC4800F144K2048,... Show More
User7795
DAVE™
Hi Infineon,

there is a bug at Dave4.4.2, at CAN app, the mask is truncated (Windows7/64):
User18515
DAVE™
I have Dave 4.4.2. I need to build the DALI code for XMC 1400. i downloaded the sample code and would like to import to a project. but it says the cod... Show More
User17893
DAVE™
Hello everybody,i recently upgraded to GCC8 according to this thread: https://www.infineonforums.com/threads/4645-Upgrading-GCC-in-DAVE4? Compiling wo... Show More
User12713
DAVE™
Hi, I want to have 4 Groups of 3 Phase PWM (not SVM, without deadtime). Which App schould I choose? Timer? CCU4? (examples) How can I make Synchronisa... Show More
User18137
DAVE™
After a small break I'm beating my head against the wall again trying to get the HTTP_SERVER_RTOS_XMC47 example to work with FATFS. I've tried the FAT... Show More
ipek
DAVE™
Is it possible to customize interrupt callbacks ? For example when an interrupt occurs I want my_func to be called instead of IRQx_Handler.
User16409
DAVE™
Hello everybody,I have analyzed a little and found that PSRAM is used by the flash code (so called RAM code) and by the CMSIS RTOS it loads and execut... Show More