DAVE™ Forum Discussions
DAVE™
Hi ,i am bit confused with the ADC_004 and IO004 Apps hardware and software connectivity ,As per my application i am interfacing current transformer t...
Show More
Hi ,i am bit confused with the ADC_004 and IO004 Apps hardware and software connectivity ,As per my application i am interfacing current transformer to ADC channel 8-bit mode ,i am using XMC1100 ARDUNIO board ,Based on the value given by ADC i supposed to on Relays,i am Keeping some voltage value as reference eg:2V ,if reference voltage is less than <2V Relay1 should be on,If reference voltage>2V Relay2 should on.please suggest me what are the Required configurations i supposed to do for ADC_004 &IO004 App.I have read the Help contents but little confusion is their please suggest me.pins as per datasheet i am using P0.4 GPIO for relay1,P0.12 ,GPIOP fo r relay2, P2.6 AA for ADC Channel.please suggest me.
Show Less
DAVE™
Hi Community,after getting a Project going with the USBCV001 App i started a new one. After debugging the new one the microcontroller is found as an u...
Show More
Hi Community,
after getting a Project going with the USBCV001 App i started a new one. After debugging the new one the microcontroller is found as an unknow device... In the other Project it went fine. The new Project is a SHa512 implementation (already implemented by someone else, took it from the internet). I need the data output for data control when i extend the existing code. The Source file ist attached (as .txt). Why does USBVC001 does not work here?
best regards
Nathan Show Less
after getting a Project going with the USBCV001 App i started a new one. After debugging the new one the microcontroller is found as an unknow device... In the other Project it went fine. The new Project is a SHa512 implementation (already implemented by someone else, took it from the internet). I need the data output for data control when i extend the existing code. The Source file ist attached (as .txt). Why does USBVC001 does not work here?
best regards
Nathan Show Less
DAVE™
hi i am try running the ADC-004,when i tried to generate Generate code it showing error as below,please let me know how to solve thisThanks&RegardsP...
Show More
hi i am try running the ADC-004,when i tried to generate Generate code it showing error as below
,please let me know how to solve this
Thanks&Regards
Prathibha Show Less
,please let me know how to solve this
Thanks&Regards
Prathibha Show Less
DAVE™
Hi,Anyone played with the resolver example : "Resolver_FOC_Motor_Example1.zip"With encoder and hall sensor is working well, but not with resolver.I ha...
Show More
Hi,
Anyone played with the resolver example : "Resolver_FOC_Motor_Example1.zip"
With encoder and hall sensor is working well, but not with resolver.
I have the right board now XMC4500 CPU_45A-V3 board and MOT_GPDLV-V2 board.
I want to readjust the parameters to run with a different motor and resolver
when i start the motor is sniping slowly (i think for auto tuning the angle). But after it`s starts to oscillate and potentiometer is not doing anything.
I tried different motor parameters but the same. I have Nanotec DB42S3 motor with 4 pole pairs.
They not specified anything about the resolver parameters like no of lobes. some are with 3 others with 4. so where i do adjust this?
I have default IQSTARTUP 2F and i do not know what is meaning.
Also the i do not know how thy calculate this value" Volt_DC 2915U "
Any help would be good.
Iulian Show Less
Anyone played with the resolver example : "Resolver_FOC_Motor_Example1.zip"
With encoder and hall sensor is working well, but not with resolver.
I have the right board now XMC4500 CPU_45A-V3 board and MOT_GPDLV-V2 board.
I want to readjust the parameters to run with a different motor and resolver
when i start the motor is sniping slowly (i think for auto tuning the angle). But after it`s starts to oscillate and potentiometer is not doing anything.
I tried different motor parameters but the same. I have Nanotec DB42S3 motor with 4 pole pairs.
They not specified anything about the resolver parameters like no of lobes. some are with 3 others with 4. so where i do adjust this?
I have default IQSTARTUP 2F and i do not know what is meaning.
Also the i do not know how thy calculate this value" Volt_DC 2915U "
Any help would be good.
Iulian Show Less
DAVE™
Hello,I keep getting into a situation where the DAVE CE view does not launch as it does after installation. It is missing the app connection diagrams ...
Show More
Hello,
I keep getting into a situation where the DAVE CE view does not launch as it does after installation. It is missing the app connection diagrams and the list to select apps for inclusion. If I try to relaunch DAVE, Open Perspective or Launch a View, it remaining unchanged. Is there some way to reset the UI so that I don't have to reinstall DAVE. I am familiar with Eclipse if there is somewhere to remove or alter files but I cannot see the ability to do anything from the GUI itself.
Thanks,
Jason Show Less
I keep getting into a situation where the DAVE CE view does not launch as it does after installation. It is missing the app connection diagrams and the list to select apps for inclusion. If I try to relaunch DAVE, Open Perspective or Launch a View, it remaining unchanged. Is there some way to reset the UI so that I don't have to reinstall DAVE. I am familiar with Eclipse if there is somewhere to remove or alter files but I cannot see the ability to do anything from the GUI itself.
Thanks,
Jason Show Less
DAVE™
I suspect that there may be a problem with either the XMC4500F144K1024 step AC silicon or the UART001 DAVE App ver 1.0.24. I am using DAVE 3.1.10. Se...
Show More
I suspect that there may be a problem with either the XMC4500F144K1024 step AC silicon or the UART001 DAVE App ver 1.0.24. I am using DAVE 3.1.10.
Sending characters to UART001 does not result in the pin P4.7 output expressing the async. serial signal. If the UART Tx pin is reassigned to P3.11 in the manual pin assignment dialog, then the resulting code does express good UART output on P3.11, as seen by an oscilloscope.
Using IO004 to toggle an output at P4.7 does work and expresses an output correctly on that pin, so this rules out a damaged pin output driver.
I have found this behavior to be repeatable on two different boards, one with a new step AC device that had never before been powered up.
A minimal DAVE 3.1.10 project reproducing this behavior is attached to this post. Perhaps another knowledgeable person could try this and see if they obtain the same results that I did.
Thanks for any help,
-Kurt Show Less
Sending characters to UART001 does not result in the pin P4.7 output expressing the async. serial signal. If the UART Tx pin is reassigned to P3.11 in the manual pin assignment dialog, then the resulting code does express good UART output on P3.11, as seen by an oscilloscope.
Using IO004 to toggle an output at P4.7 does work and expresses an output correctly on that pin, so this rules out a damaged pin output driver.
I have found this behavior to be repeatable on two different boards, one with a new step AC device that had never before been powered up.
A minimal DAVE 3.1.10 project reproducing this behavior is attached to this post. Perhaps another knowledgeable person could try this and see if they obtain the same results that I did.
Thanks for any help,
-Kurt Show Less
DAVE™
Hi there
Is it possible to write a own dave app? If this works how?
Thanks for your help!
Is it possible to write a own dave app? If this works how?
Thanks for your help!
DAVE™
Hello Sophia,what about an app which represents another Dave Project (links to it), so that one could create several "sub" projects, which the solver ...
Show More
Hello Sophia,
what about an app which represents another Dave Project (links to it), so that one could create several "sub" projects, which the solver would include in (at least) its pin mapping process?
If this isn't planned already, please take this as a feature request 🙂
BR,
Daniel Show Less
what about an app which represents another Dave Project (links to it), so that one could create several "sub" projects, which the solver would include in (at least) its pin mapping process?
If this isn't planned already, please take this as a feature request 🙂
BR,
Daniel Show Less
DAVE™
Hi i am trying with XMC2GO i am trying to debug the ADC_004 App in DAVE 3.1.10 not able to generate code under this option solve and regenerate code...
Show More
Hi i am trying with XMC2GO i am trying to debug the ADC_004 App in DAVE 3.1.10 not able to generate code under this option solve and regenerate code option showing error ,error as failed to update one or more resources in the application model please see the error log for more information,in error log the message is failed to generate file ADC_004 confc.c Reason:Failed to initialize ADC_004 confc.jet templete file,please let me know how to solve
Thanks&Regards
Prathibha Show Less
Thanks&Regards
Prathibha Show Less
DAVE™
I have an issue with the breakpoints. Every time I set a break point it appears with a cross slash over the little point and the check mark.I'm sure ...
Show More
I have an issue with the breakpoints. Every time I set a break point it appears with a cross slash over the little point and the check mark.
I'm sure I'm downloading the debug configuration and it is also set as the active one but the break points don't work at all.
I'm using the j link from segger.
Breakpoints were working before but suddenly they stopped working.
thanks Show Less
I'm sure I'm downloading the debug configuration and it is also set as the active one but the break points don't work at all.
I'm using the j link from segger.
Breakpoints were working before but suddenly they stopped working.
thanks Show Less