DAVE™ Forum Discussions
DAVE™
HelloI did a quick test with Dave4. After a brief look I like the more user-friendly naming of the apps and various interface items, but I also hit th...
Show More
Hello
I did a quick test with Dave4. After a brief look I like the more user-friendly naming of the apps and various interface items, but I also hit the following problem.
I created a DaveCE project and added a PWM app, without any extra code, and this leads to a compilation error. The default make process is started with -j4 as argument and I would like to remove it, to simplify the debugging and pinpoint the compilation error. How could I do this, as I did not find a way to edit the arguments for make.
Thank you! Show Less
I did a quick test with Dave4. After a brief look I like the more user-friendly naming of the apps and various interface items, but I also hit the following problem.
I created a DaveCE project and added a PWM app, without any extra code, and this leads to a compilation error. The default make process is started with -j4 as argument and I would like to remove it, to simplify the debugging and pinpoint the compilation error. How could I do this, as I did not find a way to edit the arguments for make.
Thank you! Show Less
DAVE™
I want to realize the demo of XMC1300 CCU4 timers slices concatenation using the apps,but the app CCU4GLOBAL seem can't realize more except initialize...
Show More
I want to realize the demo of XMC1300 CCU4 timers slices concatenation using the apps,but the app CCU4GLOBAL seem can't realize more except initialize the MCLK of CCU4.I find an alike example of XMC4K just like the pictures below.
XMC1300 CCU4
XMC4K UART Show Less
XMC1300 CCU4
XMC4K UART Show Less
DAVE™
how to set the correct path,the properity of the file displays "path: /XMC1300-CCU4-Concatenation/MCUINIT/MCUInit.h","Location: E:\DAVE\XMC1300-CCU4...
Show More
how to set the correct path,the properity of the file displays "path: /XMC1300-CCU4-Concatenation/MCUINIT/MCUInit.h","Location: E:\DAVE\XMC1300-CCU4-Concatenation\MCUINIT\MCUInit.h" or ../Startup/startup_XMC1300.s:40:59: fatal error: ../Dave/Generated/inc/DAVESupport/Device_Data.h: No such file or directory.
Thank you. Show Less
Thank you. Show Less
DAVE™
Hi,I got around my PWMSP001/ADC001 problems by switching to ADC002 and having the PWM service routine queue entries to the ADC. That seems to be worki...
Show More
Hi,
I got around my PWMSP001/ADC001 problems by switching to ADC002 and having the PWM service routine queue entries to the ADC. That seems to be working fine.
I am still having the problems with RTC001 not triggering the service interrupt. I looked at the RTC001 example and modified it to use RTC001_Enable() and it works fine. So it looks just about the same as my code except I have all sorts of other things that *should not* matter to the RTC.
I have the same problem with SYSTM timers not calling their interrupt routines.
Can someone please help. I am happy to post the entire project if that would help.
thanks,
jerry Show Less
I got around my PWMSP001/ADC001 problems by switching to ADC002 and having the PWM service routine queue entries to the ADC. That seems to be working fine.
I am still having the problems with RTC001 not triggering the service interrupt. I looked at the RTC001 example and modified it to use RTC001_Enable() and it works fine. So it looks just about the same as my code except I have all sorts of other things that *should not* matter to the RTC.
I have the same problem with SYSTM timers not calling their interrupt routines.
Can someone please help. I am happy to post the entire project if that would help.
thanks,
jerry Show Less
DAVE™
Can I still use code like#if UC_ID == 4206 # define CODRV_CANCLOCK_80MHZ#else# error "CPU type not set"#endif#define CODRV_DEBUGmy first set up leads ...
Show More
Can I still use code like
my first set up leads to
or
It looks like uc_id.h is not anymore available. Show Less
#if UC_ID == 4206
# define CODRV_CANCLOCK_80MHZ
#else
# error "CPU type not set"
#endif
#define CODRV_DEBUG
my first set up leads to
error: #error "CPU type not set"
or
#if UC_SERIES == XMC42 || UC_SERIES == XMC41
It looks like uc_id.h is not anymore available. Show Less
DAVE™
Hi,What is the ideal app to receive an analog signal in the I / O XMC1100, make a treatment / conversion and transmit the Tx UART?BR,Taina T.
Show More
Hi,
What is the ideal app to receive an analog signal in the I / O XMC1100, make a treatment / conversion and transmit the Tx UART?
BR,
Taina T. Show Less
What is the ideal app to receive an analog signal in the I / O XMC1100, make a treatment / conversion and transmit the Tx UART?
BR,
Taina T. Show Less
DAVE™
Hi All,Using DAVE 3.1.10 , APPs is V1.0.66 , JLINK Driver is V4.96Customer doesn't work(Title) at above DAVE development system.Do we support it?Thank...
Show More
Hi All,
Using DAVE 3.1.10 , APPs is V1.0.66 , JLINK Driver is V4.96
Customer doesn't work(Title) at above DAVE development system.
Do we support it?
Thanks.
Best Regards,
Dennies Chu Show Less
Using DAVE 3.1.10 , APPs is V1.0.66 , JLINK Driver is V4.96
Customer doesn't work(Title) at above DAVE development system.
Do we support it?
Thanks.
Best Regards,
Dennies Chu Show Less
DAVE™
Why can't I select the Portpins 2.2 to 2.9 for digital Input with Dave Manual Pin Assignment?
Kind regards
Ewald
Kind regards
Ewald
DAVE™
Hi,I have an issue regarding include file configuration:I need to configure my own include paths under properties -> C/C++ General -> Paths and Symbol...
Show More
Hi,
I have an issue regarding include file configuration:
I need to configure my own include paths under properties -> C/C++ General -> Paths and Symbols -> Includes.
After adding a new Dave App to the project and running code generation, my custom paths are removed from the list of include directories.
After re-configuring my custom settings, compilations works fine.
Is there a way to prevent Dave from removing my configuration or to somehow circumvent this issue?
Kind regards,
Christian Show Less
I have an issue regarding include file configuration:
I need to configure my own include paths under properties -> C/C++ General -> Paths and Symbols -> Includes.
After adding a new Dave App to the project and running code generation, my custom paths are removed from the list of include directories.
After re-configuring my custom settings, compilations works fine.
Is there a way to prevent Dave from removing my configuration or to somehow circumvent this issue?
Kind regards,
Christian Show Less
DAVE™
Hello,I'm starting to develop a project with the XMC1100, but is the first time I use Dave software. My goal is to generate a PWM output with a change...
Show More
Hello,
I'm starting to develop a project with the XMC1100, but is the first time I use Dave software. My goal is to generate a PWM output with a change of the analog signal will go into a I/O XMC1100. Can anyone tell me if there is a similar example of such a project? App or what should I use for this project?
Thanks
Taina Show Less
I'm starting to develop a project with the XMC1100, but is the first time I use Dave software. My goal is to generate a PWM output with a change of the analog signal will go into a I/O XMC1100. Can anyone tell me if there is a similar example of such a project? App or what should I use for this project?
Thanks
Taina Show Less