Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

DAVE™ Forum Discussions

Sort by:
Francesco_Lelli
DAVE™
Good morning, I'm trying to configure the POSIF peripheral to read the position from an encoder. I'm facing a problem setting the RUN bit. After I've ... Show More
Anonymous
DAVE™
I can't creat any of the Dave Projects in my virtual Maschine (vmware ). It's a Windows 7 64 bit System.The Problem is that I can insert like in the s... Show More
Anonymous
DAVE™
I have installed DAVE 4.4.2. I need the link to download DAVE SDK. I searched on the website and was not able to find it.I cannot find any options ins... Show More
Translation_Bot
DAVE™
Hi   DAVE App "EVENT_GENERATOR" for ERU has only single "pattern" and no "tout" output.According to the reference manual, OGU in ERU has 4 signals to ... Show More
Anonymous
DAVE™
Hello,i want to connect a 16x2 LCD Display ( like this ) to my XMC 4500.How can i programm it in Dave 3?Haven't found any guides for Dave, just for ar... Show More
Jedison01
DAVE™
Hi, I am looking for a description of all HW Signal Connections for all the DAVE APPs, where can I find these? Thanks, Jedison Show More
Subasri
DAVE™
HI, I'm using XMC4400 F100K512 BA Board and I'm using Dave V3.1.10 software. I have debug my first code and it is showing an error message like I have... Show More
ajana1986
DAVE™
Needed sample code for DAVE™ IDE to drive L9825 Driver IC with daisy chain connectivity, Outputs are not coming, unable to set register's bits of driv... Show More
User12216
DAVE™
When I switch and build a Release configuration, DAVE deletes the Debug directory. When I switch and build a Debug configuration, the Release director... Show More
mrtn-t
DAVE™
Hi, I have very odd problem: test code that works as "main.c" does not work as "main.cpp"I have PCB with XMC4700 an SD card connected over SPI (pins M... Show More