Not applicable
Jan 30, 2013
02:30 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 30, 2013
02:30 AM
Hi,
My target is the Hitex XMC HiLight board which is XMC4500F144x1024 so I though I should be OK up to 0x100000 bytes of flash However when I construct a simply program that goes beyond 0x3FFFF I end up with a bus fault.
I've constructed the simplest example I can think of, flashing one LED
Am missing something obvious like a linker option?
Best regards,
Andy
My target is the Hitex XMC HiLight board which is XMC4500F144x1024 so I though I should be OK up to 0x100000 bytes of flash However when I construct a simply program that goes beyond 0x3FFFF I end up with a bus fault.
I've constructed the simplest example I can think of, flashing one LED
#include//Declarations from DAVE3 Code Generation (includes SFR declaration)
#define RED_LED_HANDLE IO004_Handle0
/* This value is OK */
static const char dummyArray[0x3DFFF] = { };
/* This value fails */
//static const char dummyArray[0x3EFFF] = { };
void delay()
{
int i;
for (i=0; i<10000000; i++)
{
}
}
int main(void)
{
DAVE_Init(); // Initialization of DAVE Apps
while(1)
{
IO004_TogglePin(RED_LED_HANDLE);
delay();
}
return 0;
}
Am missing something obvious like a linker option?
Best regards,
Andy
Labels
- Tags:
- IFX
3 Replies
Jan 31, 2013
01:27 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 31, 2013
01:27 AM
Hi Andy,
I have just tried on my Hexagon board with the same device.
I have no problem with 0x3EFFF.
Actually I don't have an Hitex board.
Could you attach the linker script ?
In attachment mine.
I have just tried on my Hexagon board with the same device.
I have no problem with 0x3EFFF.
Actually I don't have an Hitex board.
Could you attach the linker script ?
In attachment mine.
/* Generated Linker Script file */
/*
* Template Version 1.0 dated 11 Oct 2012
*/
OUTPUT_FORMAT("elf32-littlearm")
OUTPUT_ARCH(arm)
ENTRY(__Xmc4500_reset_cortex_m)
GROUP(-lxmclibcstubs)
MEMORY
{
FLASH_1_cached(RX) : ORIGIN = 0x08000000, LENGTH = 0x100000
FLASH_1_uncached(RX) : ORIGIN = 0x0C000000, LENGTH = 0x100000
PSRAM_1(!RX) : ORIGIN = 0x10000000, LENGTH = 0x10000
DSRAM_1_system(!RX) : ORIGIN = 0x20000000, LENGTH = 0x10000
DSRAM_2_comm(!RX) : ORIGIN = 0x30000000, LENGTH = 0x8000
}
stack_size = 2048;
SECTIONS
{
/* TEXT section */
.text : AT(ORIGIN(FLASH_1_uncached))
{
sText = .;
*(.Xmc4500.reset);
*(.Xmc4500.postreset);
*(.XmcStartup);
*(.text .text.* .gnu.linkonce.t.*);
/* ARM <->THUMB interworking */
*(.glue*)
*(.v4*)
*(.vfp11_veneer)
/* C++ Support */
KEEP(*(.init))
__preinit_array_start = .;
KEEP (*(.preinit_array))
__preinit_array_end = .;
__init_array_start = .;
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array))
__init_array_end = .;
KEEP (*crtbegin.o(.ctors))
KEEP (*(EXCLUDE_FILE (*crtend.o) .ctors))
KEEP (*(SORT(.ctors.*)))
KEEP (*crtend.o(.ctors))
KEEP(*(.fini))
__fini_array_start = .;
KEEP (*(.fini_array))
KEEP (*(SORT(.fini_array.*)))
__fini_array_end = .;
KEEP (*crtbegin.o(.dtors))
KEEP (*(EXCLUDE_FILE (*crtend.o) .dtors))
KEEP (*(SORT(.dtors.*)))
KEEP (*crtend.o(.dtors))
/* Exception handling support */
__extab_start = .;
*(.ARM.extab* .gnu.linkonce.armextab.*)
. = ALIGN(4);
__extab_end = ABSOLUTE(.);
} > FLASH_1_cached
/* Exception handling, exidx needs a dedicated section */
.ARM.exidx ABSOLUTE(__extab_end): AT(__extab_end | 0x04000000)
{
__exidx_start = .;
*(.ARM.exidx* .gnu.linkonce.armexidx.*)
. = ALIGN(4);
__exidx_end = ABSOLUTE(.);
} > FLASH_1_cached
/* CONST data section */
.rodata ABSOLUTE(__exidx_end): AT(__exidx_end | 0x04000000)
{
*(.rodata .rodata.*)
*(.gnu.linkonce.r*)
} > FLASH_1_cached
. = ALIGN(16);
/* End of RO-DATA and start of LOAD region for DATA */
eROData = . | 0x04000000;
/* DSRAM layout (Lowest to highest)*/
/* Fully Descending Stack <-> BSS <-> DATA <-> HEAP */
/* Dummy section for stack */
Stack (NOLOAD) :
{
. = . + stack_size;
__Xmc4500_stack = .;
} > DSRAM_1_system
Communication_Buffers :
{
*DMA_Descriptors.o (COMMON);
} > DSRAM_2_comm
/* BSS section */
.bss :
{
__Xmc4500_sBSS = .;
* (.bss);
* (.bss*);
* (EXCLUDE_FILE(*DMA_Descriptors.o) COMMON);
*(.gnu.linkonce.b*)
__Xmc4500_eBSS = ALIGN(4);
} > DSRAM_1_system
/* Yes, the size must be kept outside */
__Xmc4500_BSS_Size = __Xmc4500_eBSS - __Xmc4500_sBSS;
/* Standard DATA and user defined DATA/BSS/CONST sections */
.data ABSOLUTE(ALIGN(16)): AT(eROData)
{
__Xmc4500_sData = .;
* (.data);
* (.data*);
*(*.data);
*(.gnu.linkonce.d*)
__Xmc4500_eData = ALIGN(4);
} > DSRAM_1_system
/* Yes, the size must be kept outside */
__Xmc4500_Data_Size = __Xmc4500_eData - __Xmc4500_sData;
/* Heap - Bank1*/
__Xmc4500_heap_start = ALIGN(8);
__Xmc4500_heap_end = ORIGIN(DSRAM_1_system) + LENGTH (DSRAM_1_system);
Heap_Bank1_Start = __Xmc4500_heap_start;
Heap_Bank1_Size = __Xmc4500_heap_end - __Xmc4500_heap_start;
Heap_Bank1_End = ABSOLUTE(__Xmc4500_heap_end);
/* Heap - Bank2 */
DSRAM2_Heap :
{
/* To host DATA in DSRAM2 above heap, please be sure to augment
* program loader code in the startup file */
Heap_Bank2_Start = .;
} > DSRAM_2_comm
Heap_Bank2_Size = LENGTH(DSRAM_2_comm) - (Heap_Bank2_Start - ORIGIN(DSRAM_2_comm));
/* Heap - Bank3 */
PSRAM_Heap :
{
/* To host DATA in PSRAM above heap, please be sure to augment
* program loader code in the startup file */
Heap_Bank3_Start = .;
} > PSRAM_1
Heap_Bank3_Size = LENGTH(PSRAM_1) - (Heap_Bank3_Start - ORIGIN(PSRAM_1));
/DISCARD/ :
{
*(.comment)
}
.stab 0 (NOLOAD) : { *(.stab) }
.stabstr 0 (NOLOAD) : { *(.stabstr) }
/* DWARF 1 */
.debug 0 : { *(.debug) }
.line 0 : { *(.line) }
/* GNU DWARF 1 extensions */
.debug_srcinfo 0 : { *(.debug_srcinfo) }
.debug_sfnames 0 : { *(.debug_sfnames) }
/* DWARF 1.1 and DWARF 2 */
.debug_aranges 0 : { *(.debug_aranges) }
.debug_pubnames 0 : { *(.debug_pubnames) }
.debug_pubtypes 0 : { *(.debug_pubtypes) }
/* DWARF 2 */
.debug_info 0 : { *(.debug_info .gnu.linkonce.wi.*) }
.debug_abbrev 0 : { *(.debug_abbrev) }
.debug_line 0 : { *(.debug_line) }
.debug_frame 0 : { *(.debug_frame) }
.debug_str 0 : { *(.debug_str) }
.debug_loc 0 : { *(.debug_loc) }
.debug_macinfo 0 : { *(.debug_macinfo) }
/* DWARF 2.1 */
.debug_ranges 0 : { *(.debug_ranges) }
/* SGI/MIPS DWARF 2 extensions */
.debug_weaknames 0 : { *(.debug_weaknames) }
.debug_funcnames 0 : { *(.debug_funcnames) }
.debug_typenames 0 : { *(.debug_typenames) }
.debug_varnames 0 : { *(.debug_varnames) }
/* Build attributes */
.build_attributes 0 : { *(.ARM.attributes) }
}
Attachments are accessible only for community members.
Not applicable
Jan 31, 2013
02:37 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 31, 2013
02:37 AM
Not applicable
Jan 31, 2013
04:36 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 31, 2013
04:36 AM
Hi,
I just remembered I have a Relax Lite board.
The code works fine on the Relax Lite board (having changed the IO004 assignment to P1.0).
Since P1.0 just goes to a header on the HiLight board I then tried the same code on the HiLight board and the code does not work.
The only difference I can think of is the debugger. On the HiLight board I am using the J-Link Lite debugger, on the Relax Lite board I am using the integral debugger.
Could this be the problem?
Kind regards,
Andy
I just remembered I have a Relax Lite board.
The code works fine on the Relax Lite board (having changed the IO004 assignment to P1.0).
Since P1.0 just goes to a header on the HiLight board I then tried the same code on the HiLight board and the code does not work.
The only difference I can think of is the debugger. On the HiLight board I am using the J-Link Lite debugger, on the Relax Lite board I am using the integral debugger.
Could this be the problem?
Kind regards,
Andy