May 16, 2014
03:22 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 16, 2014
03:22 AM
Update, May, 16, 2014
The following updates for DAVE are now available for download:
1. An update of DAVE eclipse plug-ins for DAVE v3.1.10
It includes fixing of deficiencies of the created gpdsc files for ARM/ Keil MDK and fixing of deficiencies when updating Device Description libraries
2. A CMSIS patch for DAVE v3.1.10
A patch of the CMSIS folder located in the installation of DAVE v3.1.10 to patch startup files, linker script templates (improve functionality and optimize memory usage) and the CMSIS DSP library.
3. DAVE Apps libraries update site has been updated to v1.0.64
- DAVEApps_Library_001 has been updated to v1.0.64
- DAVEApps_MotorControl_Library_001 has been updated to v1.0.28
- DAVEApps_Lighting_Library_001 v1.0.16 (no change)
- DAVEApps_HMI_Library_001 has been updated to v1.0.4
- Device Description libraries have been updated to release 2014-05-09
This DAVE App libraries update contains:
8 new DAVE Apps: 3 new DAVE Apps to build applications with the high resolution PWM peripheral and 5 new USB Apps that improves USB drivers and a clearer separation between driver, device class and application layer.
15 DAVE Apps have been updated to fix deficiencies.
25 Device Description libraries have been updated.
More details and instructions to perform the update.
Example Projects
In the coming 2 weeks we will update a large number of examples to the most recent version of DAVE Apps and we will add new examples for the high resolution PWM Apps and the new USB Apps These example projects can be searched and downloaded directly in DAVE or separately as zip file from this web page.
Free Keil / ARM µVsion MDK for XMC1000.
Please note, that the latest version of Keil / ARM µVision MDK can be downloaded for free. It is a perpetual Version limited to use it for XMC1000.
The following updates for DAVE are now available for download:
1. An update of DAVE eclipse plug-ins for DAVE v3.1.10
It includes fixing of deficiencies of the created gpdsc files for ARM/ Keil MDK and fixing of deficiencies when updating Device Description libraries
2. A CMSIS patch for DAVE v3.1.10
A patch of the CMSIS folder located in the installation of DAVE v3.1.10 to patch startup files, linker script templates (improve functionality and optimize memory usage) and the CMSIS DSP library.
3. DAVE Apps libraries update site has been updated to v1.0.64
- DAVEApps_Library_001 has been updated to v1.0.64
- DAVEApps_MotorControl_Library_001 has been updated to v1.0.28
- DAVEApps_Lighting_Library_001 v1.0.16 (no change)
- DAVEApps_HMI_Library_001 has been updated to v1.0.4
- Device Description libraries have been updated to release 2014-05-09
This DAVE App libraries update contains:
8 new DAVE Apps: 3 new DAVE Apps to build applications with the high resolution PWM peripheral and 5 new USB Apps that improves USB drivers and a clearer separation between driver, device class and application layer.
15 DAVE Apps have been updated to fix deficiencies.
25 Device Description libraries have been updated.
More details and instructions to perform the update.
Example Projects
In the coming 2 weeks we will update a large number of examples to the most recent version of DAVE Apps and we will add new examples for the high resolution PWM Apps and the new USB Apps These example projects can be searched and downloaded directly in DAVE or separately as zip file from this web page.
Free Keil / ARM µVsion MDK for XMC1000.
Please note, that the latest version of Keil / ARM µVision MDK can be downloaded for free. It is a perpetual Version limited to use it for XMC1000.
- Tags:
- IFX
0 Replies