Attachments are accessible only for community members.
Jun 08, 2021
02:07 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jun 08, 2021
02:07 AM
Hello,
I am trying to implement a TCP client on the XMC4800. This client should be able to send individual messages to a Server and to receive the response messages.
For the beginning, I worked with the "IOT_EXAMPLE_XMC47" and implemented this example for a XMC4800. Also, I removed some functions which I don't need for the communication. I have this source code so far:
I use Wireshark to analyze the network communication between the XMC and my PC. But the TCP connection always resets and I don't know why. Maybe because my PC is not working for a host?
I also tried to connect the XMC with Putty (RAW Connection type), but that doesn't work either. Besides, I do get a ping response form the XMC.*
PS: I hope you can open the zip attachment wich includes the project.
Thank you for your help!
Regards,
Maxi
I am trying to implement a TCP client on the XMC4800. This client should be able to send individual messages to a Server and to receive the response messages.
For the beginning, I worked with the "IOT_EXAMPLE_XMC47" and implemented this example for a XMC4800. Also, I removed some functions which I don't need for the communication. I have this source code so far:
I use Wireshark to analyze the network communication between the XMC and my PC. But the TCP connection always resets and I don't know why. Maybe because my PC is not working for a host?
I also tried to connect the XMC with Putty (RAW Connection type), but that doesn't work either. Besides, I do get a ping response form the XMC.*
PS: I hope you can open the zip attachment wich includes the project.
Thank you for your help!
Regards,
Maxi
0 Replies