Sep 29, 2016
10:00 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 29, 2016
10:00 AM
Today we published a patch release of 2 new DAVE APPs to fix recent identified issues:
E_EEPROM_XMC1:
When migrating a project that includes this APP to another device the memory size was not correctly given, this has been fixed.
MULTICAN_CONFIG:
Coded generation issue when using multiple message objects has been fixed, also the help document has been improved.
The updated DAVE APP release note contains more details.
How to install the updated APPs.
When starting DAVE an update notification will appear.
To start the update manually Press:
Help ->Check for DAVE APP Updates
An updated zip with all DAVE Apps to install/ update them offline can also be downloaded.
In the meantime also most of the DAVE Example projects are updated to the latest DAVE APP releases plus a couple of new examples are released:
Further examples will be released next week.
E_EEPROM_XMC1:
When migrating a project that includes this APP to another device the memory size was not correctly given, this has been fixed.
MULTICAN_CONFIG:
Coded generation issue when using multiple message objects has been fixed, also the help document has been improved.
The updated DAVE APP release note contains more details.
How to install the updated APPs.
When starting DAVE an update notification will appear.
To start the update manually Press:
Help ->Check for DAVE APP Updates
An updated zip with all DAVE Apps to install/ update them offline can also be downloaded.
In the meantime also most of the DAVE Example projects are updated to the latest DAVE APP releases plus a couple of new examples are released:
- USB Host examples for mass storage or SW update
- HSB Device Examples for SW update
- EtherCAT Example for SW update
Further examples will be released next week.
- Tags:
- IFX
0 Replies