Not applicable
May 18, 2014
01:43 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 18, 2014
01:43 AM
Hi all,
i have some questions according thread creation of the RTOS001 App (Version 1.0.24).
In the thread Definition there is a Parameter "instance". The documentation sais: "number of posible instances".
The questions are:
How can i start the instances of a thread, or will they all be started during "osKernelStart"?
How can i get the instance number of a certain thread during runtime, or will i get different ThreadIds for different instances?
Is it possible to Hand over different arguments to the thread instances during creation?
Is it also possible to create different threads (multiple calls of "osThreadCreate") with the same execution function each with instance = 1?
Thanks for help
Thomas
i have some questions according thread creation of the RTOS001 App (Version 1.0.24).
In the thread Definition there is a Parameter "instance". The documentation sais: "number of posible instances".
The questions are:
How can i start the instances of a thread, or will they all be started during "osKernelStart"?
How can i get the instance number of a certain thread during runtime, or will i get different ThreadIds for different instances?
Is it possible to Hand over different arguments to the thread instances during creation?
Is it also possible to create different threads (multiple calls of "osThreadCreate") with the same execution function each with instance = 1?
Thanks for help
Thomas
- Tags:
- IFX
5 Replies
Not applicable
May 19, 2014
01:48 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 19, 2014
01:48 AM
Hi Thomas,
You may get some hints from "RTOS001_Example1".
BR,
Zain
You may get some hints from "RTOS001_Example1".
BR,
Zain
Not applicable
May 19, 2014
12:12 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 19, 2014
12:12 PM
Zain wrote:
Hi Thomas,
You may get some hints from "RTOS001_Example1".
BR,
Zain
Hi Zain,
thanks for the replay but unfortionally this example creates two threads with different thread functions with instance=1. So this is not what i am locking for.
Thanks
Thomas
Attachments are accessible only for community members.
May 20, 2014
02:58 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 20, 2014
02:58 AM
Hi Thomas,
The parameter 'number of instances' at thread definition, allows multiple threads to execute the same function.
Find attached an example that shows:
1. How to define multiple threads sharing the same function.
2. Identification of the running thread at run time.
3. Passing an argument to the thread.
4. Retarget printf to use SWO (you will need SEGGER JLink SWO Viewer tool)
5. Use of nanolib
At thread definition it is required to specify the function to be run, number of instances and stack size.
The threads are pushed into the READY list (among other preparation steps) using osThreadCreate.
You will need to start the scheduler (osKernelStart) so that the threads get scheduled and moved to the RUNNING state (only one at a time).
Best regards,
Jesus
The parameter 'number of instances' at thread definition, allows multiple threads to execute the same function.
Find attached an example that shows:
1. How to define multiple threads sharing the same function.
2. Identification of the running thread at run time.
3. Passing an argument to the thread.
4. Retarget printf to use SWO (you will need SEGGER JLink SWO Viewer tool)
5. Use of nanolib
At thread definition it is required to specify the function to be run, number of instances and stack size.
The threads are pushed into the READY list (among other preparation steps) using osThreadCreate.
You will need to start the scheduler (osKernelStart) so that the threads get scheduled and moved to the RUNNING state (only one at a time).
Best regards,
Jesus
Not applicable
May 21, 2014
03:40 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 21, 2014
03:40 AM
jferreira wrote:
Hi Thomas,
The parameter 'number of instances' at thread definition, allows multiple threads to execute the same function.
Find attached an example that shows:
1. How to define multiple threads sharing the same function.
2. Identification of the running thread at run time.
3. Passing an argument to the thread.
4. Retarget printf to use SWO (you will need SEGGER JLink SWO Viewer tool)
5. Use of nanolib
At thread definition it is required to specify the function to be run, number of instances and stack size.
The threads are pushed into the READY list (among other preparation steps) using osThreadCreate.
You will need to start the scheduler (osKernelStart) so that the threads get scheduled and moved to the RUNNING state (only one at a time).
Best regards,
Jesus
Hi Jesus,
many thanks for the very percise answer. This is exactly what i am looking for.
There are two Question left:
1.
Is it possible to assign different stack sizes as well ?
2.
Is it possible to change the priority of the threads before calling osKernelStart?
In may application the thread functions are all the same, but the call trees, starting from "thread" (that means, the threads calling different functions with different stack requirements), are very different. So i have a need to assign different stack sizes and different priorities to each instance but keep the same thread function.
Many thanks for your effort
Thomas
May 26, 2014
01:04 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 26, 2014
01:04 AM
Hi Thomas,
Unfortunately, to my knowledge, there is no way to specify different stack size for threads sharing the same function.
Furthermore changing dynamically the stack size of a thread it is not supported. It is defined statically at compilation time.
On the other hand, it is possible to change the priority at run time using osThreadSetPriority (osThreadId thread_id, osPriority priority).
Best regards,
Jesus
Unfortunately, to my knowledge, there is no way to specify different stack size for threads sharing the same function.
Furthermore changing dynamically the stack size of a thread it is not supported. It is defined statically at compilation time.
On the other hand, it is possible to change the priority at run time using osThreadSetPriority (osThreadId thread_id, osPriority priority).
Best regards,
Jesus