Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

DAVE™ Forum Discussions

Markus_S
Level 2
Level 2
10 sign-ins 5 questions asked First question asked
I have a XMC1402T038 and according to the Pinouttool V.2.1.10 can connect a full-duplex uart to pins P0.14 and P0.15.
However I can't choose those same pins in the DAVE full-duplex UART app (manual Pin allocator).
SWD is on P1.2/P1.3.
Shouldn't the two tools agree?
0 Likes
2 Replies
jferreira
Employee
Employee
First like received 750 replies posted 500 replies posted
Hi,

They do agree. Check in the CPU_XMC1_CTRL APP, you most probably have selected for the debug interface the SWD0. Which reserves the pins P0.14 and P0.15 for SWDIO and SWDCLK respectively.
Therefore you can not use them for UART. If you change the debug interface to SWD1, then you will be able to use the P0.14 and P0.15 for the UART fullduplex.
Regards,
Jesus
0 Likes
Markus_S
Level 2
Level 2
10 sign-ins 5 questions asked First question asked
Hi Jesus,
your are right. Thanks for the hint.

Regard,
Markus
0 Likes