Not applicable
Feb 20, 2015
04:43 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 20, 2015
04:43 PM
Hello,
I'm starting to develop a project with the XMC1100, but is the first time I use Dave software. My goal is to generate a PWM output with a change of the analog signal will go into a I/O XMC1100. Can anyone tell me if there is a similar example of such a project? App or what should I use for this project?
Thanks
Taina
I'm starting to develop a project with the XMC1100, but is the first time I use Dave software. My goal is to generate a PWM output with a change of the analog signal will go into a I/O XMC1100. Can anyone tell me if there is a similar example of such a project? App or what should I use for this project?
Thanks
Taina
- Tags:
- IFX
4 Replies
Not applicable
Feb 23, 2015
01:46 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 23, 2015
01:46 AM
Hi Taina,
You may take a reference to "PWM_PulseCount_Example_XMC11", "ADC004_Example1_XMC11" & "ADC002_Example 1".
BR,
Zain
You may take a reference to "PWM_PulseCount_Example_XMC11", "ADC004_Example1_XMC11" & "ADC002_Example 1".
BR,
Zain
Not applicable
Feb 24, 2015
05:36 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 24, 2015
05:36 AM
Hello, Zain
I got run the two examples of the way I need, with the correct variations of the PWM example PWM_PulseCount_Example_XMC11 and also generate a hex varying the analog input in the example ADC002_Example 1.
Now would only need to unite the two functions. Do you have a tip to help me? Must I start a project from blank and state the functions of the two examples? Or is there an easier way?
Thank you very much.
Best regards
Taina T.
I got run the two examples of the way I need, with the correct variations of the PWM example PWM_PulseCount_Example_XMC11 and also generate a hex varying the analog input in the example ADC002_Example 1.
Now would only need to unite the two functions. Do you have a tip to help me? Must I start a project from blank and state the functions of the two examples? Or is there an easier way?
Thank you very much.
Best regards
Taina T.
Not applicable
Feb 24, 2015
11:45 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 24, 2015
11:45 PM
Hi Taina,
You can't simply unite the two functions.
If you are using XMC1100, then "ADC004_Exampl1_XMC11" can be used to expand for your project. Take reference to "PWM_PulseCount_Example_XMC11" on the configuration of PWM generation.
BR,
Zain
You can't simply unite the two functions.
If you are using XMC1100, then "ADC004_Exampl1_XMC11" can be used to expand for your project. Take reference to "PWM_PulseCount_Example_XMC11" on the configuration of PWM generation.
BR,
Zain
Not applicable
Feb 28, 2015
11:35 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 28, 2015
11:35 AM
Hi, Zain
Thanks for the information. Helped me a lot to finish the PWM design.
It all worked out.
Now I will start the second part of the project, using a data transmission via UART, I will open another topic for this issue.
BR,
Taina T.
Thanks for the information. Helped me a lot to finish the PWM design.
It all worked out.
Now I will start the second part of the project, using a data transmission via UART, I will open another topic for this issue.
BR,
Taina T.