Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User6412
Level 4
Level 4
Hello All,

I think the problem I want to draw attention is very common for Dave Apps. It is pretty often the situation when the given App should be additionally reconfigured by the user, because the Apps are constrained in many aspects. I thought it is very logically to assume that all necessary initializations of the hardware units take place in DAVE_Init() function. As an example the PWMMP001 App do it through PWMMP001_Init() function wich itself called from DAVE_Init() function. But! God knows why the TRAP enable is changed inside the PWMMP001_Start() function. This is absolutely absurdly. The appropriate settings taken in additional user reconfiguration functions are lost. I think, this is not a good approach and should be changed possibly sooner.

Thanks for attention
0 Likes
1 Reply
Georg_Huba
Employee
Employee
Hi Dimitry, thanks for this input, our expert will look into it, then we will respond.
Georg
0 Likes