Not applicable
Jun 21, 2018
02:48 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jun 21, 2018
02:48 AM
Hi all,
I have configerated an IO ports as external interrupt source and have used the IO002 App (DAVE-3).
The signal is connected via a EUR001 instance to the NVIC.

In ERU001 App I can configurate the Event Trigger Logic with e.g. "falling edge" detection, but my Software will also trigger the external signal on the rising edge!
Have someone seen the same behaivour with DAVE3 or have you any ideas, how I can fix this Problem?
Thanks in advance,
I have configerated an IO ports as external interrupt source and have used the IO002 App (DAVE-3).
The signal is connected via a EUR001 instance to the NVIC.
In ERU001 App I can configurate the Event Trigger Logic with e.g. "falling edge" detection, but my Software will also trigger the external signal on the rising edge!
Have someone seen the same behaivour with DAVE3 or have you any ideas, how I can fix this Problem?
Thanks in advance,
0 Replies