Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

DAVE™ Forum Discussions

Georg_Huba
Employee
Employee
Today we published new versions of DAVE, DAVE APPs, XMC Lib, Device Descriptions, and Device Support Pack.

DAVE v4.4.2
New features:

  • Board selection option introduced.
  • Library store default path is moved to DAVE package
  • DAVE package is upgraded from Eclipse Luna to Neon package
  • Please note that DAVE 4.4.2 is coming as zip file without installer (details in the installation instructions


Download New DAVE v4.4.2
Download DAVE 4.4.2 release note

The SDK for DAVE v4.4.2 will be released later.


DAVE APPs
25 DAVE APPs have been updated (fixing of issues, adding new features, update)
CCU4_SLICE_CONFIG, CCU8_SLICE_CONFIG, CLOCK_XMC1, CMSIS_DSP, CMSIS_RTOS_RTX, CRC_SW, DAC_LUT, E_EEPROM_XMC4, ECAT_SSC, ETH_LWIP, FATFS, FREERTOS, GLOBAL_POSIF, GLOBAL_SCU_XMC1, GLOBAL_SCU_XMC4, HTTP_SERVER, I2C_MASTER, I2C_SLAVE, PMSM_FOC, PWM_BC, PWM_SVM, RTC, SPI_MASTER, UART_CONFIG, VADC_GLOBAL_CONFIG

Contributed DAVE APPs
2 DAVE APPs have been updated: SEGGER_RTT, UCPROBE

Download release note (contains also the changes of the contributed DAVE APPs)
Please note, a user action is required when migrating an existing project to the new version of the UART_CONFIG APP (described in the release note).

DAVE Device Description
The device descriptions for the XMC1400 series and the XMC4300 series have been updated with missing connectivity and alternate function options.
Download release note

DAVE Device Pack v2.2.2
Update to XMC Lib v2.1.18
Update to CMSIS 5.2.0
Support for new devices added
Board Support added (can only be us along with DAVE v4.4.2 and not with earlier DAVE version)
Updates of CMSIS startup and system files

Download release note

Download the complete library update sites as zip file for DAV 4.4.2 (is already included when downloading the new DAVE 4.4.2 version).
Download the complete library store for DAVE v4.3.2 and older Versions (without board support schemes).


XMC Lib v2.1.18
15 XMC Libs are updated:
Common, CAN, CCU4, CCU8, DMA, ETH_MAC, FCE, FLASH, GPIO, I2C, MATH, UART, USIC, SCU, VADC
Download release note
Download XMC Lib v 2.1.18 package

The current web sites of DAVE are not full updated, this will happen within the next couple of day.

Also the CMSIS PACKs for XMC100 and XMC4000 have been updated.
They can be directly updated from the web using the PACK installer in the respective tools.
Or can be downloaded separately as PACK files:
XMC1000 PACK

XMC4000 PACK
0 Likes
0 Replies