Not applicable
Feb 22, 2017
01:28 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 22, 2017
01:28 PM
Hello,
I'm new to the DAVE and XMC programming.
today I installed DAVE and the Segger J-Link drivers on my pc. (64-bit Version)
It went through without any problems. Then I downloaded and installed the dave APPS and wanted to make this tutorial with the XMC2GO: http://www.infineon.com/dgdl/Infineon-DAVE_Quick_Start-GS-v02_00-EN.pdf?fileId=5546d4624cb7f111014d0...
When I want to do the pin mapping part, it is not possible because all the pins are greyed out:

Also, the manual pin allocator doesn't work either:

So, I can't put the PWM-Signal on a GPIO-Pin.
When I close DAVE and want to continue with the project, I always get this error: Error occured while connecting to the solver process
I can click OK and continue, but the previous described problems remain. The error is also shown, when I'm importing existing projects.
I tried running without antivirus, without firewall and with admin rights. I also tried several uninstallations and installations of DAVE 32bit and 64bit and the J-Link drivers.
On my other PC I tried also. The problem is not there! Only on this PC.
Can someone help me find the problem?
Thanks in advance!
Best regards.
I'm new to the DAVE and XMC programming.
today I installed DAVE and the Segger J-Link drivers on my pc. (64-bit Version)
It went through without any problems. Then I downloaded and installed the dave APPS and wanted to make this tutorial with the XMC2GO: http://www.infineon.com/dgdl/Infineon-DAVE_Quick_Start-GS-v02_00-EN.pdf?fileId=5546d4624cb7f111014d0...
When I want to do the pin mapping part, it is not possible because all the pins are greyed out:
Also, the manual pin allocator doesn't work either:
So, I can't put the PWM-Signal on a GPIO-Pin.
When I close DAVE and want to continue with the project, I always get this error: Error occured while connecting to the solver process
I can click OK and continue, but the previous described problems remain. The error is also shown, when I'm importing existing projects.
I tried running without antivirus, without firewall and with admin rights. I also tried several uninstallations and installations of DAVE 32bit and 64bit and the J-Link drivers.
On my other PC I tried also. The problem is not there! Only on this PC.
Can someone help me find the problem?
Thanks in advance!
Best regards.
- Tags:
- IFX
0 Replies