Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Not applicable
I have an XMC4400 with the Ethernet (COM) and OLED (HMI) boards. I installed Dave 3.1.8 and the "September 2013" release of the samples.

I'm trying to find an Ethernet-enabled example which uses DHCP to configure the Ethernet port on the COM board. I've looked at WEBSERVER001_Example1 and WEBSERVER001_Example2, as well as a slew of "Model" and "Generated" files within those two projects and can't find a way to modify either of those examples to use DHCP. I tried the same thing with the ETH004 example and any file changes I made were either ignored, overwritten, or resulted in compile time errors that shouldn't have happened based on the changes I made.

The problem I'm trying to solve is that my house LAN is 192.168.0/24 and the office LAN is 10.10/16. The default static IP address of 192.168.0.10 is fine (the gateway is wrong -- my gateway is 192.168.0.1 and the examples are configured for 192.168.0.10) for the house, as I don't have anything on that IP address at the moment, but it won't work at all at the office.
1 Reply
Not applicable
Never mind -- I launched the IDE in the "Dave IDE" perspective instead of "Dave CE". Once in "Dave CE" mode I was able to reconfigure the "ETH004" thingy to use DHCP. I rebuilt the project and all is well -- the XMC4400 made a DHCP request, was assigned 192.168.0.208 (my DHCP block starts at 192.168.0.100 or so), and proceeded to do all the appropriate networking stuff.
0 Likes