Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Georg_Huba
Employee
Employee
DAVE v4 and DAVE APPs are now released as Productive version.
Also a new version of XMC Lib has been released.


DAVE v4.1.2 and DAVE SDK v4.1.2
With this new version, DAVE v4 and DAVE SDK has reached Productive status.
Major improvements in comparison to the previous version are.

  • Fixing of issues and design improvements
  • Feature to upgrade to new versions of DAVE APPs
  • Feature to reserve resources to avoid resources conflicts between DAVE APPs and other SW components
  • Improved APP management: Clear differentiation between Productive and Beta APPs
  • DAVE SDK: improved debug capabilities
  • Support of the Cortex M3 based TLE9800 microcontrollers (including library , no APPs)
DAVE v4.1.2 requires a new workspace and a new local library store. Projects from DAVE v4.0.0 can be imported

More information:
Overview of Improvements of DAVE v4
DAVE Release Note
Download DAVE v4.1.2
1443.attach

DAVE APPs and Device Descriptions.
In total now 70 DAVE APPs are released, most of them (58) are released as Productive version: 12 APPs are released as Beta version.

  • 8 new DAVE APPs are released: ACMP_CONFIG , COMP_REF, COMP_SLOP_GEN, CMSIS_RTOS_RTX, CMSIS_DSP, DAC_SWEEP, FREERTOS and GLOBAL_ACMP.
  • ACMP_CONFIG is a peripheral configuration APP that creates the initialization function of the peripheral module based on a graphical GUI, to operate the peripheral the APIs from the peripheral driver can be used
  • 4 DAVE APPs for motor control uses cases have been removed, because they will undergo significant improvements: BLDC_SCALAR_CTRL, HALL_POSIF, PMSM_FOC, PMSM_SCALAR_CTRL

All Device descriptions have been updated (fixing of issues and improvements the solver interface. Because of these changes a local library store with DSVE v4.0.0 cannot be used with DAVE v4.1.2 (default location path has been changed)

18 DAVE APPs of this release package are not fully upward compatible to their earlier beta version. However DAVE v4.0.0 projects can be imported in DAVE v4.12 and upgraded, the incompatible APPs require some manual adjustments.
For most of the DAVE APPs there are examples available, they can be downloaded directly from DAVE.

Further information:
Guide how to move projects from DAVE v4.0.0 to DAVE v4-1-2
Release Note DAVE APPs
Release Note DAVE Device Descriptions
Download the update site package as separate zip file
The release history of each APP can be found in the APP documentation

XMC Lib
The XMC lib has been update to version 2.0.0. In this version, peripheral driver for Ethernet and DSD module have been added. The complete change log can be found in the release note and in the XMC lib documentation. 4 peripheral drivers are not fully upward compatible. However, existing user code can be easily ported with a few manual actions (details are described in the guide to move projects from DAVE v4.0.0 to DAVE v4.1.2).

Further information
Release Note
XMC Lib as separate package including documentation examples and the CMSIS files



The next update is planned by end of October 2015
3 Replies
Not applicable
May I know what is planed to be included for the next release?
0 Likes
User2235
Level 3
Level 3
Hi,

Are there plans for a lwip example for XMClib (not DAVE APP) to use with EWARM?

Ari.
0 Likes
User9154
Level 4
Level 4
Hi Mr.Huba,
I have do it all, but by afterwork like / check for updates...
I got a message: 1441.attach

BR
zbyno
0 Likes