Not applicable
Sep 18, 2013
02:29 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 18, 2013
02:29 AM
You can use SPI001Configure () API to switch control of multiple SPI slaves with different configurations:
1) Input the "Number of chip select lines" required in the "SPI001 Configuration" tab
2) Do manual pin assignment for "ChipSelectA" & "ChipSelectB" etc
3) Use SPI001Configure () API to pass several parameters at one time
1) Input the "Number of chip select lines" required in the "SPI001 Configuration" tab
2) Do manual pin assignment for "ChipSelectA" & "ChipSelectB" etc
3) Use SPI001Configure () API to pass several parameters at one time
0 Replies