Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Not applicable
To create external interrupt functionality the ERU Apps are required.

There are two ERU Apps available:
1) ERU001 App provides External Request Trigger configuration functionality
2) ERU002 App provides connectivity options configuration for Pattern detection and Output Trigger Gating

ERU001 App needs be combined with ERU002 App to provide a full use case.

The DAVE example project "External Intr ERU001_ERU002_Example2" demonstrates a simple application use case.
0 Replies