Not applicable
Sep 23, 2013
12:05 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 23, 2013
12:05 AM
PWMMP001 App is designed to generate the Multi phase (2 or 3 or 4 phase) centre aligned, asymmetric PWM waveforms with dead time.
1) CC8 slices are from the same module either CCU80 or CCU81
2) Up to 2 PWM outputs per Timer Slice (OUTy0 & OUTy1) due to asymmetric PWM
In "xmc4500_rm_v1+2_2012_12_", Figure 23-28 shows the "Centre Aligned Asymmetric mode scheme".
Workaround:
Use PWMMP001 App as a baseline, manually configure the OUTy2 & OUTy3.
What was planned:
A new PWM App provides the configuration of generating 4 PWM outputs from one CCU8x slice.
1) CC8 slices are from the same module either CCU80 or CCU81
2) Up to 2 PWM outputs per Timer Slice (OUTy0 & OUTy1) due to asymmetric PWM
In "xmc4500_rm_v1+2_2012_12_", Figure 23-28 shows the "Centre Aligned Asymmetric mode scheme".
Workaround:
Use PWMMP001 App as a baseline, manually configure the OUTy2 & OUTy3.
What was planned:
A new PWM App provides the configuration of generating 4 PWM outputs from one CCU8x slice.
0 Replies