Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Not applicable
Hi Friends,

I:Dn watchdog example when i run it after counter becomes five it does not reset the program but jumps to the following code...of startup_xmc4500.s
file at line no labeled 2 and does not goes away from the instruction...please tell the solution....
/**************startup_xmc4500.s******************* ***/

/* ================== START OF VECTOR ROUTINES ============================= */
.thumb
/* ================================================== ====================== */
/* Reset Handler */

.thumb_func
.globl __Xmc4500_reset_cortex_m
.type __Xmc4500_reset_cortex_m, %function
__Xmc4500_reset_cortex_m:
.fnstart

1. /* Disable Branch prediction */
2. LDR R0,=PREF_PCON
3. LDR R1,[R0]
4. ORR R1,R1,#0x00010000
5. STR R1,[R0]

........
.............
..........
....................
2 Replies
ron
Employee
Employee
Hello mohan,

We analyzed the topic. In fact what you see is a WDT Reset. The CPU do not jump, you can check the register RSTSTAT and you will see that the flag for the WDT Reset is set. Be aware the bitfield shows the accumulated reset status. This means you will find as well a PORST Reset.
You are using the Segger J Link right. One way to run the code is to do some single Step and the go back to run mode after the reset happen. This behavior is currently checked with the debugger vendor. Other debugger not behave like that so we think it's a debugger issue.
The second way is to clear the reset status bits. To do so include the following line inside the code:

...
DAVE_Init();


RESETn = RESET001_GetResetInfo(); //To get the information of the last reset
RESETn &=WDT_RESET; //Mask for WDT reset
SCU_RESET->RSTCLR |= 0x1; // clear reset info if(!(RESETn))
{
WDT001_Enable();
...


This will change the behavior in the way that the CPU will not halt anymore at the reset handler. you can put a breakpoint on the included line and you will see that the WDT reset happen.

Ron
0 Likes
Not applicable
ron wrote:
You are using the Segger J Link right. One way to run the code is to do some single Step and the go back to run mode after the reset happen. This behavior is currently checked with the debugger vendor. Other debugger not behave like that so we think it's a debugger issue.

Do you have any news on that?
0 Likes