Community Translations Forum Discussions
Hi,
I'd like to translate KBA90926 into Japanese.
Please confirm to my work.
moto
Original KBA: KBA90926
Sleep Timer as a Wake-Up Source in PSoC® 3 and PSoC 5LP – KBA90926
Show LessHi,
I'd like to translate KBA227565 into Japanese.
Please confirm to my work.
moto
Original KBA: KBA227565
Power Sequence for PSoC 6 – KBA227565
Show LessHello,
I would like to translate "Flash Read Protection for Bootloader and Bootloadable Code in PSoC® 4", please confirm to my work.
Best Regards,
Naoaki Morimoto
Show LessHi,
I'd like to translate KBA93082 into Japanese.
Please confirm to my work.
moto
Original KBA: KBA93082
Working of the PSoC® 3/5LP RTC Without a Power Supply and Across Resets – KBA93082
Show LessI tried to translate this KBA.
Please confirm.
Thanks,
Tetsuo
質問:
FX3S、SD3、SD2とそれらのリファレンスデザインの機能の違いは何ですか?
回答:
FX3S、SD3、およびSD2は2つのストレージカードをサポートします。 ただし、これらのデバイスには、1枚のストレージカードのみをサポートするものもあります。
ファミリ名 | Part Number | USB 3.0 | USB 2.0 | P-Port | データシート |
FX3S | CYUSB3035 | サポート | サポート | サポート | |
SD3 | CYUSB3025 | サポート | サポート | 未サポート | |
SD2 | CYUSB2025 | 未サポート | サポート | 未サポート |
FX3Sベースのリファレンスデザインが2つ、こちらにあるFX3SのWebサイトのKitsセクションから参照できます。SD3とSD2はFX3Sの派生類似品のため、これらのデバイスでもFX3Sのリファレンスデザインを参考にすることができます。
1. FX3S RAID-on-Chip USB Dongle - このキットはCYUSB3035が実装されており、FX3SのRAID1機能のデモに使用できます。SDインタフェースは双方4bitのみをサポートしています。
2. FX3S DVK - このキットはCYUSB3035が実装されており、FX3Sの機能を実証するために使用されます。 このキットでは、の2つの8bitストレージポートをサポートしており、SD3.0、SDIO3.0、eMMC 4.41が対応可能です。8bitのSDコネクタが実装されています。SDソケットと互換性のあるeMMCパドルボードを使用して、eMMCを評価することができます。また、P-portコネクタもあり、FPGAやアプリケーションプロセッサを接続することができます。
Show Less