Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Community Translation - Unit of A/D Conversion Error in Traveo S6J3XXX Series and CY9D560 Series MCUs – KBA227498

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,               

I would like to translate KBA227498 into Japanese.

Please confirm to my work.

Thanks,

Kenshow

0 Likes
2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello, Kenshow-san

Confirm to work this KBA.

Thanks

Jenna

Jenna Jo
0 Likes

Hi Jenna-san,

                                

Japanese translation was over.
Please check below.

Original KBA:

Unit of A/D Conversion Error in Traveo S6J3XXX Series and CY9D560 Series MCUs – KBA227498

Thanks.

Kenshow

==============================

タイトル: Traveo S6J3XXXシリーズおよびCY9D560シリーズMCUのA/D変換エラーの単位– KBA227498

バージョン:**

質問:

データシートでは、LSBA/D変換誤差の単位として使用しています。LSBがエラーの単位として使用されるのはなぜでしょうか?

回答:

サイプレスMCUでは、AD変換エラーはLSB(最下位ビット)の単位で測定されます。したがって、AD変換エラーはLSB単位で表されます。たとえば、10 V A / Dコンバータで0 Vから5 Vの入力範囲を変換する場合、ビットあたりの電圧は「(1/1024x 5です。誤差が±4LSBの場合、A / Dコンバータの変換結果には「±4×1/1024×5の誤差が含まれます。

この設定は、以下の一連のTraveo MCUに適用されます。

  • S6J3110
  • S6J3120
  • S6J3200
  • S6J3300
  • S6J3350
  • S6J3360
  • S6J3370
  • S6J3400
  • S6J3510
  • CY9D560

注:
製品のプレフィックスMBCYに変更されました。たとえば、MB9D5XXCY9D5XXに変更されました。

==============================

10-June-2020

Kenshow

0 Likes