Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
keni_4440091
Level 7
Level 7
500 replies posted 100 solutions authored 50 solutions authored

Dear supporter

I want to translate the following KBA. Please confirm to my work.

Understanding the VLKO parameter in parallel NOR flash - KBA233942

Regards,

Nino

0 Likes
3 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Nino-san

Confirm to work this KBA.

Thanks.

Best Regards, 

Jenna Jo
0 Likes

Dear Jenna

The following shows the translated version in Japanese for targeted KBA.

Please conform and double check.

Regards,

Nino

---------------------------------------------------------------------------------------------------

パラレルNOR flashのVLKOパラメータを理解する – KBA233942

 

Version: **

 

VLKOはコア電源供給(VCC)のロックアウト電圧です。VLKOの目的は、VCCパワーアップおよびパワーダウンの移行時の間で意図しないプログラム/消去動作を避けるために、プログラム/消去前にデバイスが期待するVCCレベルにある事を確認することです。VCCがVLKOを下回る時、flashメモリアレイ全体は、プログラムまたは消去動作に対して保護されます。これにより、電源移行時にメモリ内容が誤って変更されることがなくなります。VLKOは、単一値の閾値パラメータで、全てのデバイスには異なるVLKOがあります。最小/最大は、VLKOの推定範囲です。全てのデバイスは、この範囲内のVLKOになります。

 

パワーダウンの間、またはVCCがVLKOを下回った場合、VCCおよびVIO電圧が再び動作範囲に上昇したときに部品が正しく初期化されるためには、tPDの期間、VCCおよびVIO電圧がVCCリセット(VRST)の最小値を下回らなければなりません。図1を参照してください。

システム実装では、全てのデバイスでVLKOに最大値を使用する必要があります。例えば、VCCの監視; VLKOを下回った場合、デバイスが正しく初期化されるように、VCCおよびVIO電圧がtPDの期間にわたってVCCリセット(VRST)の最小値を下回っていることを確認してください。

 

keni_4440091_1-1634611709405.png

1.パワーダウンおよび電圧降下

 

図1にパワーダウンおよび電圧降下図およびVLKOを示します。S29GL01G/512T データシートRev.Lの図1を参照してください。

この図は、全てのインフィニオンGLシリーズパラレルNOR flashファミリに適用します。

 

Labels   Memory: NOR Flash

Tags: datasheet GL-N gl-p gl-s gl-t interface max min nor flash parallel pl-j Power-down timing vcc VLKO voltage levels VS-R 

Add tags

0 Likes
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Nino-san

Thank you for updates.

I will let you know there is any issues.

Thanks,

Jenna 

Jenna Jo
0 Likes